This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678数据传输速度



请问:C6678的L2和L3到DDR3的数据传输速度理论上可以达到多大啊?

  • 您好,

    LL2的理论数据总线吞吐量为16GBps,SL2对外的理论数据总线吞吐量为64GBps,DDR对外数据总线理论吞吐量为12.8GBps。从上述可以看到SL2的对外总线吞吐量甚至高于LL2,但是由于SL2到core中间还有MSMC等,所以实际cpu访问SL2的吞吐量还受限于中间相关总线的带宽及速率。具体可以查看C66x corepac user guide进行分析。

    LL2、L3及DDR之间的数据交换,可以使用DSP Core,EDMA,IDMA,packetDMA完成,每种方式的传输速率不一样。根据实测结果来看对于DDR与LL2和SL2的数据交换建议采用EDMA3吞吐量最大,在1GHz主频下,对于DDR与LL2的交换吞吐量可达5.3GBps,DDR与SL3的交换吞吐量达10GBps。

    请参考!

  • Andy Yin:

    你好,

    你所说的L2、LL2、SL2、L3、SL3应该各不相同,但是现在对这些缩略语或者名词有点不太清楚,能给详细介绍下吗?

    另外,还有L1P、L1D、L1Cache、L1、L2、L2Cache、L1SRAM、L2SRAM、MSMC之间又有什么的关系和不同,他们的配置或者组织结构情况是什么样的?

    多谢!

  • 您好,

    L2: local memory;   SL2: shared memmory; SL3: 通过MSMC将SL2可以重映射成SL3;

    关于各个memory的关系及差异,可以查看corepac的文档,其中有详细的解释。