This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM3730 部分板子不能从SD启动

Other Parts Discussed in Thread: DM3730, TPS65930

用DM3730的片子做了一批板子,有一些板子插上SD不能正常启动,基本信息如下:

1.SYS_BOOT信号设置没有问题
2.26M与32.768K信号正常
3.PMIC使用的是TPS65930,各个信号按照TI的参考设计
4.上电后IIC1有动作,然后PMIC的VMMC1输出3.0V正常
5.UART3输出 60 ,测试CPU的MMC1在上电后只有CLKO有信号输出

6.测试CPU的MMC1在上电后只有CLKO有信号输出
但其他几个信号,例如CMD ,DATA0--DATA3无信号

 

这个输出的数字:60 到底是什么意思?