This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP型号的选择



您好,我要用DSP做模式识别/图像重构。DSP接收FPGA采集来的数据,并在内部完成模式识别/图像重构后,与上位机进行通信。请问完成这些功能选择哪种型号的DSP可以,性价比比较高

  • wang hongmei您好,

    建议可以考虑使用定浮点C66x,C66x core支持1.25GHz主频,同时提供了丰富的运算指令;并且提供多种DSP型号可供选择,有单核,双核,4核,8核;该系列DSP对外提供多个高速接口如SRIO, PCIe等,方便与FPGA高速通信。

    具体请参考www.ti.com/.../device.page,谢谢!