This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCC中调节rgb2rgb遇到的问题

TI工程师你好:

现在使用的软件是Appro的ipnc_rdk3.5版本,在使用DCC2.0.4调节dm8127下sensor的图像质量时,发现调节rgb2rgb的机制与ITT软件不同,像ITT软件在调节rgb2rgb完成后将不同色温下(使用了5个色温作为基准)的颜色转换矩阵记录下来,一次将所有基准色温调节完成后,将各色温矩阵写入代码中就算调节完成了;而dm8127并没有使用代码写入参数,而是直接使用DCC将调试参数实时导入相机的方式来实现rgb2rgb的调节的。现在我做了两种尝试:第1种,我依次将各个色温下做了rgb2rgb调节,同时每做依次调节,就实时的导入到相机中,最终发现寄存器中rgb2rgb参数在不同色温下一直是最后一个,自我总结认为前四个调节的rgb2rgb在相机中被最后一组参数覆盖了;第2种,在“photospace regions”界面将ColorTemperature分成了5分范围依次为0 - 3000,3001-4000,4001-5000,5001-6500,6501-7500,同时将其依次设置成调整类为0、1、2、3、4,然后依次对每个色温执行“Process Plugin”操作,所有色温执行完一遍后执行“Export DCC profile binary”,然后直接导入到相机中,然后在色温箱下分部测试不同色温,发现rgb2rgb的值仍然是一种即7500K的值。

请问TI工程师,我对RGB2RGB的调试方法哪里有问题呢?

  • 自己顶一下!上面的问题已经解决了,但是出现了另一个问题:rgb2rgb是在特定色温下调节的,但是实际上调节后的每一组数值却应用到一个范围的色温下(比如,某组rgb2rgb应用于6000K-6900K的色温中),请问这么大的色温范围而使用相同的rgb2rgb会不会出现偏色问题呢?