This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

基于6467t平台VPIF问题

您好,请问6467t的vpif是否支持两路高清输入,采用一路高清在vpif口8位的方式进入,另一路高清在另外一个vpif口8位方式进入。

  • 你好,

    DM6467T的VPIF输入时钟最高是150Mhz,理论上是可以输入两路1080p30的图像,但似乎DM6467T本身无法编码两路1080p30,我认为输入也是没有意义的。而且DDR使用的带宽也会急剧增加,导致系统性能下降。

  • 您好,感谢您的及时回复。

    是这样,我们想输入两路1080i50的视频,每一路都是8位输入。时钟是150MHz。我们在VPIF采集完两路高清数据后,不会直接进行高清编码,而是会转变成D1的格式在进行编码,这样就可以编两路了。

    请问如果vpif输入两路高清的话,有没有配置的demo。

    谢谢您。