平台:exynos4412
问题:拍照或者录像时,每帧图像的前面32行和前面64列的像素点都是黑色的
我把寄存器16H写0x60(默认为0x80),前面64列像素点正常了,但是后面64列编程黑色了。请帮忙分析一下,多谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
看看这几个寄存器:
AVID start/stop 看看是否踩得一行点数足够。
lines per frame, 看看你踩得行数是否足够。
[ 48.725138] tvp5150: Video input source selection #1 = 0x00
[ 48.740171] tvp5150: Analog channel controls = 0x15
[ 48.755151] tvp5150: Operation mode controls = 0x00
[ 48.770125] tvp5150: Miscellaneous controls = 0x6f
[ 48.785164] tvp5150: Autoswitch mask= 0x00
[ 48.800143] tvp5150: Color killer threshold control = 0x10
[ 48.845135] tvp5150: Luminance processing controls #1 #2 and #3 = 60 00 00
[ 48.865165] tvp5150: Brightness control = 0x80
[ 48.880208] tvp5150: Color saturation control = 0x80
[ 48.895120] tvp5150: Hue control = 0x00
[ 48.910156] tvp5150: Contrast control = 0x80
[ 48.925134] tvp5150: Outputs and data rates select = 0x40
[ 48.940176] tvp5150: Configuration shared pins = 0x02
[ 48.970128] tvp5150: Active video cropping start = 0x0000
[ 49.000137] tvp5150: Active video cropping stop = 0x0000
[ 49.015183] tvp5150: Genlock/RTC = 0x01
[ 49.030155] tvp5150: Horizontal sync start = 0x80
[ 49.045127] tvp5150: Vertical blanking start = 0x00
[ 49.060171] tvp5150: Vertical blanking stop = 0x00
[ 49.090117] tvp5150: Chrominance processing control #1 and #2 = 0c 54
[ 49.110159] tvp5150: Interrupt reset register B = 0x00
[ 49.125130] tvp5150: Interrupt enable register B = 0x00
[ 49.140171] tvp5150: Interrupt configuration register B = 0x00
[ 49.155146] tvp5150: Video standard = 0x00
[ 49.185162] tvp5150: Chroma gain factor: Cb=0xca Cr=0x92
[ 49.200137] tvp5150: Macrovision on counter = 0x0f
[ 49.215112] tvp5150: Macrovision off counter = 0x01
[ 49.230156] tvp5150: ITU-R BT.656.4 timing(TVP5150AM1 only)
[ 49.260169] tvp5150: Device ID = 5151
[ 49.290120] tvp5150: ROM version = (hex) 01.00
[ 49.320139] tvp5150: Vertical line count = 0x0271
[ 49.335110] tvp5150: Interrupt status register B = 0x87
[ 49.350148] tvp5150: Interrupt active register B = 0x00
[ 49.425163] tvp5150: Status regs #1 to #5 = 7e 08 0b 77 83
[ 49.429167] tvp5150: Teletext filter 1 reg 0xb1 = 00 00 00 00 00
[ 49.505129] tvp5150: Teletext filter 2 reg 0xb6 = 00 00 00 00 00
[ 49.595112] tvp5150: Teletext filter enable = 0x00
[ 49.610110] tvp5150: Interrupt status register A = 0xc0
[ 49.625124] tvp5150: Interrupt enable register A = 0x00
[ 49.640263] tvp5150: Interrupt configuration = 0x04
[ 49.655111] tvp5150: VDP status register = 0x40
[ 49.670121] tvp5150: FIFO word count = 0x00
[ 49.685117] tvp5150: FIFO interrupt threshold = 0x80
[ 49.700113] tvp5150: FIFO reset = 0x00
[ 49.715117] tvp5150: Line number interrupt = 0x00
[ 49.745111] tvp5150: Pixel alignment register = 0x004e
[ 49.760123] tvp5150: FIFO output control = 0x01
[ 49.775125] tvp5150: Full field enable = 0x00
[ 49.790112] tvp5150: Full field mode register = 0x7f
[ 49.793634] tvp5150: CC data reg 0x90 = 00 00 00 00
[ 49.855141] tvp5150: WSS data reg 0x94 = 00 00 00 00 00 00
[ 49.945133] tvp5150: VPS data reg 0x9a = 00 00 00 00 00 00 00 00
[ 50.065132] tvp5150: VPS data reg 0xa2 = 00 00 00 00 00
[ 50.140238] tvp5150: VITC data reg 0xa7 = 00 00 00 00 00 00 00 00 00
[ 50.275123] tvp5150: Line mode reg 0xd0 = ff ff ff ff ff ff ff ff
[ 50.395131] tvp5150: Line mode reg 0xd8 = ff ff ff ff ff ff ff ff
[ 50.515125] tvp5150: Line mode reg 0xe0 = ff ff ff ff ff ff ff ff
[ 50.635124] tvp5150: Line mode reg 0xe8 = ff ff ff ff ff ff ff ff
[ 50.755121] tvp5150: Line mode reg 0xf0 = ff ff ff ff ff ff ff ff
[ 50.875132] tvp5150: Line mode reg 0xf8 = ff ff ff ff
这些是寄存器读出来的值