研究生生毕设要选芯片,做些数据处理,练练手,主流推荐的单核C6000是什么啊
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
目前的主流推荐是定浮点C66x系列DSP,可选的型号包括c6670/1/2/4/8,具备高达1.25GHz的主频,提供丰富的指令,包括支持复乘、矩阵运算等高级指令,同时具有丰富的高速外设接口,便于与外设进行高速通信。具体可以参考www.ti.com/.../device.page%E8%BF%9B%E8%A1%8C%E5%9E%8B%E5%8F%B7%E6%AF%94%E8%BE%83,相关具体的学习开发资料请参考:
基于Keystone 架构的高性能多核C6678/C6670系列DSP在线资源汇总
推荐TMS320C6713
TMS320C6713 是美国TI于1997年推出的C6000系列DSP芯片的一款,它是32位高速浮点型DSP,时钟最高频率为300MHz。
TMS320C6713主要特点有:
(1)体系结构采用超长指令字(VLIW)结构,单指令字长为32位,指令包里有8个指令,总字长达到256位。执行指令的功能单元已经在编译时分配好,程序运行时通过专门的指令分配模块,可以将每个256位的指令包同时分配到8个处理单元,并由8个单元同时运行。其最大处理能力可以达到2400MIPS。
(2)采用二级缓冲处理,4KByte直接匹配的程序缓冲L1P,4KByte可匹配的数据缓冲L1D,256KByteL2额外匹配内存。32位外部存储器接口,可无缝连接SRAM、EPROM、Flash、SBSRAM和SDRAM。
(3)丰富的外设,包括DMA,EDMA,支持无需CPU参与可以在允许的地址空间里传送数据,扩展总线,具有主机口和I/O端口操作等功能,多通道缓冲串口,其通过配置能和多种串行通信接口通信,两个32位通用定时器等。3