你好
我们使用的平台是tda4ve j721s2 平台,我们在8.4版本的sdk上面已经验证好了摄像头,现在切换到了8.5版本的sdk,运行摄像头的时候出现了下面的错误,请帮忙看一下
App Create Graph Done!
832.018575 s: VX_ZONE_ERROR:[ownContextSendCmd:802] Command ack message returned failure cmd_status: -1
832.018627 s: VX_ZONE_ERROR:[ownContextSendCmd:838] tivxEventWait() failed.
832.018635 s: VX_ZONE_ERROR:[ownNodeKernelInit:525] Target kernel, TIVX_CMD_NODE_CREATE failed for node capture_node
832.018642 s: VX_ZONE_ERROR:[ownNodeKernelInit:526] Please be sure the target callbacks have been registered for this core
832.018648 s: VX_ZONE_ERROR:[ownNodeKernelInit:527] If the target callbacks have been registered, please ensure no errors are occurring within the create callback of this kernel
832.019155 s: VX_ZONE_ERROR:[ownGraphNodeKernelInit:583] kernel init for node 0, kernel com.ti.capture ... failed !!!
832.019169 s: VX_ZONE_ERROR:[vxVerifyGraph:2055] Node kernel init failed
832.019175 s: VX_ZONE_ERROR:[vxVerifyGraph:2109] Graph verify failed
[MCU2_0] 832.017828 s: [UDMA]
[MCU2_0] 832.017867 s: [Error] RM PSI Pairing failed!!!
[MCU2_0] 832.017893 s: [UDMA]
[MCU2_0] 832.017919 s: [Error] UDMA channel paring failed!!
[MCU2_0] 832.017964 s: src/csirx_drvUdma.c @ Line 246:
[MCU2_0] 832.017990 s: [ERROR]UDMA channel open FAILED!!!
[MCU2_0] 832.018024 s: src/csirx_drv.c @ Line 1544:
[MCU2_0] 832.018049 s: [ERROR]UDMA channel close FAILED!!!
[MCU2_0] 832.018080 s: src/csirx_drv.c @ Line 1544:
[MCU2_0] 832.018104 s: [ERROR]UDMA channel close FAILED!!!
[MCU2_0] 832.018133 s: src/csirx_drv.c @ Line 1544:
[MCU2_0] 832.018156 s: [ERROR]UDMA channel close FAILED!!!
[MCU2_0] 832.018186 s: src/csirx_drv.c @ Line 1544:
[MCU2_0] 832.018209 s: [ERROR]UDMA channel close FAILED!!!
[MCU2_0] 832.018238 s: src/csirx_drv.c @ Line 402:
[MCU2_0] 832.018262 s: Create failed for given configuration
[MCU2_0] 832.018294 s: src/fvid2_drvMgr.c @ Line 759:
[MCU2_0] 832.018317 s: Driver create failed!!
[MCU2_0] 832.018352 s: VX_ZONE_ERROR:[tivxCaptureCreate:1206] : Capture Create Failed!!!
期待回复