从本论坛下载的DDR3的例子程序,调用的是Memory_test工程。例程本身没有XXCML文件(似乎是这个后缀名,初学CCS5,记不大清了,反正就是配置文件),自己新建一个,选用Simulator, 6678板子,或者是Emulator, 6678。另外,包含的CSL头文件都改为6678路径下的。编译都报个错误:can not use STABS debug options with 6400+/6740/6600。帮忙解答下,多谢!
另外问下,这个工程能否在6678L的开发板上跑?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
lei tang,
您好!
编译和硬件配置文件没有关系。我使用下面的编译选项可以编译。希望能够有帮助。看看你的环境中是否有-gp选项,如果有的话,去掉试试。
-mv6600 -g -O3 --include_path="C:/Program Files/Texas Instruments/ccsv51/ccsv5/tools/compiler/c6000/include" --include_path="C:/workspace_v5_1/Memory_Test/../common" --include_path="C:/PC:/Program Files/Texas Instruments/pdk_c6618_1_0_0_5/packages" --include_path="C:/Program Files/Texas Instruments/pdk_c6618_1_0_0_5/packages/ti/csl" --diag_warning=225 --big_endian --abi=eabi