This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

在自己制作的板子上启动时,会出现arm uboot启动失败的情况,具体详情如下:


经过跟踪发现arm是在从msmc跳转到ddr时卡死了
代码
void board_init_f (ulong bootflag)
{
....
gd->bd->bi_baudrate = gd->baudrate;
/* Ram ist board specific, so move it to board code ... */
dram_init_banksize();
display_dram_config(); /* and display it */

gd->relocaddr = addr;
gd->start_addr_sp = addr_sp;
gd->reloc_off = addr - _TEXT_BASE;
debug ("relocation Offset is: %08lx\n", gd->reloc_off);

memcpy (id, (void *)gd, sizeof (gd_t));
/* 这两行是我调试添加的
dram_compare(id,(void *)gd, sizeof (gd_t));//比较了一下源数据和目的数据,没有发现区别
debug("stack:&addr(0x%x),addr(0x%lx),id(0x%lx),addr_sp(0x%lx)\n",
&addr,addr,id,addr_sp);
*/
relocate_code (addr_sp, id, addr);---->进入到start.S

/* NOTREACHED - relocate_code() does not return */

}
cong start.S--->board_init_r

void board_init_r (gd_t *id, ulong dest_addr)
{
char *s;
bd_t *bd;
ulong malloc_start;

debug ("========\n");

...
}
没有发现board_init_r中的打印输出,说明卡死在start.S中了

打印信息如下:
U-Boot 2011.06-02.01.00.01-svn (Nov 29 2013 - 14:12:34)

U-Boot code: 0C001000 -> 0C05580C BSS: -> 0C066B70
I2C: ready
monitor len: 00065B70
ramsize: 18000000
TLB table at: bfff0000
Top of RAM usable for U-Boot at: bfff0000
Reserving 406k for U-Boot at: bff8a000
Reserving 4352k for malloc() at: bfb4a000
Reserving 24 Bytes for Board Info at: bfb49fe8
Reserving 120 Bytes for Global Data at: bfb49f70
New Stack Pointer is: bfb49f60
RAM Configuration:
Bank #0: a8000000 384 MiB
relocation Offset is: b3f89000
stack:&addr(0xc000f74),addr(0xbff8a000),id(0xbfb49f70),addr_sp(0xbfb49f60)

注意的一点是当init_ddr3 初始化一次的时候每次都是卡死在这个地方
但是当init_ddr3 初始化两次的时候,十次能有2-3次boot正确启动。