This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS3.3 优化编译时的编译选项通过命令行如何输入



软件版本:CCS3.3

PC操作系统:win7

芯片:C6747

问题描述:通过看TI的优化编译文档,提供了很多的编译选项,可是不知道在哪里输入这些编译选项。eg:cl6x file.c file2.c --run_linker --rom-model --outputfile = prog.out --library=rts6747.lib

我只知道可以通过ccs中的bulid option菜单来添加选项,但是这里的命令行就不太懂了。我试着运行了cgtool目录下的cl6x.exe.但弹出的界面一闪而逝。

所以请教:

1.通过命令行来编译,具体如何操作。最好能举个例子。

2.TI是否有相关的文档。小弟愚昧,可能是没找对文档。

万分感谢!