This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP C5502 EMIF 外部存储器连接问题

C5502 EMIF 的地址线为什么是从A2开始,是否因为5502是32位数据总线的原因?使得一次寻址为4Byte。

参考设计中的C5502使用的一片32bit的SDRAM,目前该料已经停产,很难买到。

我想替换成一片之前使用过的16bit位宽的SDRAM,是否有问题。地址线应如何连接,是否还是从A2开始,BE0~BE3应该如何与两个DQM相连。BA片选线的连接?另外软件上是否也要做相应的修改?

C5502 EMIF与CFI接口的Nor Flash连接,CE信号线是否有特定要求,从ROM里的bootloder启动后跳转到的初始地址是否需要使用对应的CE线来实现。

望赐教!