This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM36x Image Tuning Tool - AWB Tuning无法产生AWB_config.cfg



请教各位,

我用的版本是ImageTuningTool_DM36x_Full_2.2,
做awb tuning时,当设置完参数按下'Tuning'按键,
在AWB_Tuning资料夹下指产生了以下档案:
1. TI_AWB_Calibration_Config.txt,
2. CbCrRGB_addi_ref.txt, CbCrRGB_ref.txt,
3. XXXX_YUV_H3A_SELECTED.txt, XXXX_RGB_H3A_SELECTED.txt, XXXX_RGB_HIGH_RES.txt, XXXX_RGB_H3A.txt,

没看到AWB_config.cfg产生,且在command line 留下以下讯息

--------------------------------------------------------------------
Checking errors in configuration settings in TI_AWB_Calibration.m...
--------------------------------------------------------------------

--------------------------------------------------------------------
No errors found in the configuration settings in TI_AWB_Calibration.m
--------------------------------------------------------------------

--------------------------------------------------------------------
Get Data Process Begins
--------------------------------------------------------------------
Input directory is: .\\
Output directory is: .\\
Total num of ref shots = 4
Ref shots are:
6500, 4800, 4000, 2800,
h3a_col = 12
h3a_row = 32
--------------------------------------------------------------------

End of processing reference 1
End of processing reference 2
End of processing reference 3
End of processing reference 4
--------------------------------------------------------------------
DATA Processing Completed Successfully
--------------------------------------------------------------------
--------------------------------------------------------------------
DATA Display Begins
--------------------------------------------------------------------

--------------------------------------------------------------------
DATA Display Completed Successfully
--------------------------------------------------------------------
--------------------------------------------------------------------
DATA Interpolation Begins
--------------------------------------------------------------------
Warning: Polynomial is badly conditioned. Add points with distinct X
values, reduce the degree of the polynomial, or try centering
and scaling as described in HELP POLYFIT.
> In polyfit at 80
In interp_ref at 37
In AWB_Interpolate at 159
In TI_AWB_Calibration at 316
MSE_1 =NaN
Warning: Polynomial is badly conditioned. Add points with distinct X
values, reduce the degree of the polynomial, or try centering
and scaling as described in HELP POLYFIT.
> In polyfit at 80
In interp_ref at 37
In AWB_Interpolate at 159
In TI_AWB_Calibration at 316
MSE_2 =NaN
Warning: Polynomial is badly conditioned. Add points with distinct X
values, reduce the degree of the polynomial, or try centering
and scaling as described in HELP POLYFIT.
> In polyfit at 80
In interp_ref at 37
In AWB_Interpolate at 159
In TI_AWB_Calibration at 316
MSE_3 =NaN
Warning: Polynomial is badly conditioned. Add points with distinct X
values, reduce the degree of the polynomial, or try centering
and scaling as described in HELP POLYFIT.
> In polyfit at 80
In interp_ref at 37
In AWB_Interpolate at 159
In TI_AWB_Calibration at 316
MSE_4 =NaN
??? Attempted to access temp(1); index out of bounds because numel(temp)=0.

MATLAB:badsubscript

-------------------------------------------------------------------------------------------------------------------------------------------

设置参数的步骤参考过DM365-Image Tuning Tool User's Guide.pdf

麻烦大家帮帮我,感谢