Dear All,
目前基于AM3517的硬件平台的内存容量为256MB,使用两片MT47H64M16 – 8 Meg x 16 x 8 banks内存芯片,现在问题是:
1)AM3517最大内存可以扩展到多少?
2)AM3517是否支持4片DDR2内存扩展?驱动能力能否带动?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear All,
目前基于AM3517的硬件平台的内存容量为256MB,使用两片MT47H64M16 – 8 Meg x 16 x 8 banks内存芯片,现在问题是:
1)AM3517最大内存可以扩展到多少?
2)AM3517是否支持4片DDR2内存扩展?驱动能力能否带动?
这个是OK的。不稳定的情况,需要看看layout,layout的原则主要在datasheet中描述。
那ODT signals should be tied off at the memory.如何理解?
在内存则加一个下拉电阻?
如果是按照图中使用一个CS的,则可以使用ODT,将其分别连接到DDR2上。
如果CS0和CS1都使用了,则ODT就不要接到DDR2,可以将ODT引脚通过电阻下拉,禁用ODT。