This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如何提高DDR3的传输频率

Other Parts Discussed in Thread: AM3354

硬件:CPU:AM3354    DDR3:H5TQ4G63AFR-PBC

使用的是第三方评估板

阅读评估板代码

#define VTP_CTRL_READY (0x1 << 5)
#define VTP_CTRL_ENABLE (0x1 << 6)
#define VTP_CTRL_START_EN (0x1)
#define DDR3_RATIO 0x80
#define CMD_FORCE 0x00 /* common #def */
#define CMD_DELAY 0x00
#define EMIF_READ_LATENCY 0x0006
#define EMIF_TIM1 0x0CCF36AB
#define EMIF_TIM2 0x265A7FDA
#define EMIF_TIM3 0x501F855F
#define EMIF_SDREF 0x0000093B
#define EMIF_SDCFG 0x61804B32
#define DDR3_DLL_LOCK_DIFF 0x1
#define DDR3_RD_DQS 0x42
#define DDR3_PHY_FIFO_WE 0x39
#define DDR3_INVERT_CLKOUT 0x0
#define DDR3_WR_DQS 0x01
#define DDR3_PHY_WR_DATA 0x3C
#define DDR3_PHY_WRLVL 0x20
#define DDR3_PHY_GATELVL 0x20
#define PHY_RANK0_DELAY 0x01
#define PHY_DLL_LOCK_DIFF 0x0
#define DDR_IOCTRL_VALUE 0x18B

得知cl=5,cwl=5,对应DDR的datasheet,

所以ddr的传输频率为667M

我想让DDR的传输频率为800M,做如下修改

将#define EMIF_SDCFG 0x61804B32 改为#define EMIF_SDCFG 0x61805332

结果发现uboot启动不起来了,串口打印如下:

U-Boot SPL 2011.09 (Dec 19 2013 - 16:53:52)
Texas Instruments Revision detection unimplemented
Booting from MMC...

请问如何修改代码,才能让DDR跑到800M?

下面再贴一下pll的配置参数

/* Put the pll config values over here */

#define OSC 24

/* MAIN PLL Fdll = 1 GHZ, */
#define MPUPLL_M_500 500 /* 125 * n */
#define MPUPLL_M_550 550 /* 125 * n */
#define MPUPLL_M_600 600 /* 125 * n */
#define MPUPLL_M_720 720 /* 125 * n */

#define MPUPLL_N 23 /* (n -1 ) *///adu modify 24 -> 23
#define MPUPLL_M2 1

/* Core PLL Fdll = 1 GHZ, */
#define COREPLL_M 1000 /* 125 * n */
#define COREPLL_N 23 /* (n -1 ) *///adu modify 24 -> 23

#define COREPLL_M4 10 /* CORE_CLKOUTM4 = 200 MHZ */
#define COREPLL_M5 8 /* CORE_CLKOUTM5 = 250 MHZ */
#define COREPLL_M6 4 /* CORE_CLKOUTM6 = 500 MHZ */

/*
* USB PHY clock is 960 MHZ. Since, this comes directly from Fdll, Fdll
* frequency needs to be set to 960 MHZ. Hence,
* For clkout = 192 MHZ, Fdll = 960 MHZ, divider values are given below
*/
#define PERPLL_M 960
#define PERPLL_N 23 //adu modify 24 -> 23
#define PERPLL_M2 5

/* DDR Freq is 166 MHZ for now*/
/* Set Fdll = 400 MHZ , Fdll = M * 2 * CLKINP/ N + 1; clkout = Fdll /(2 * M2) */
#if (CONFIG_AM335X_EVM_IS_13x13 == 1)
#define DDRPLL_M 166 /* M/N + 1 = 25/3 */
#else
#define DDRPLL_M /*266*/303
#endif

#define DDRPLL_N 23 //adu modify 24 -> 23
#define DDRPLL_M2 1

static void ddr_pll_config(void)
{
u32 clkmode, clksel, div_m2;

clkmode = __raw_readl(CM_CLKMODE_DPLL_DDR);
clksel = __raw_readl(CM_CLKSEL_DPLL_DDR);
div_m2 = __raw_readl(CM_DIV_M2_DPLL_DDR);

/* Set the PLL to bypass Mode */
clkmode = (clkmode & 0xfffffff8) | 0x00000004;
__raw_writel(clkmode, CM_CLKMODE_DPLL_DDR);

while ((__raw_readl(CM_IDLEST_DPLL_DDR) & 0x00000100) != 0x00000100);

clksel = clksel & (~0x7ffff);
clksel = clksel | ((DDRPLL_M << 0x8) | DDRPLL_N);
__raw_writel(clksel, CM_CLKSEL_DPLL_DDR);

div_m2 = div_m2 & 0xFFFFFFE0;
div_m2 = div_m2 | DDRPLL_M2;
__raw_writel(div_m2, CM_DIV_M2_DPLL_DDR);

clkmode = (clkmode & 0xfffffff8) | 0x7;
__raw_writel(clkmode, CM_CLKMODE_DPLL_DDR);

while ((__raw_readl(CM_IDLEST_DPLL_DDR) & 0x00000001) != 0x1);
}

/*

* Configure the PLL/PRCM for necessary peripherals
*/
void pll_init()
{
// mpu_pll_config(MPUPLL_M_500);
mpu_pll_config(MPUPLL_M_720);
core_pll_config();
per_pll_config();
ddr_pll_config();
/* Enable the required interconnect clocks */
interface_clocks_enable();
/* Enable power domain transition */
power_domain_transition_enable();
/* Enable the required peripherals */
per_clocks_enable();
}