Part Number: TDA4VM
Hi, TI experts
I want to use the ptp4l tool to synchronize the time, but the synchronization failed.
I took a look at the file
Then refer to this link 3.2.2.12.3.1. PTP — Processor SDK Linux for J721e Documentation
I used two TDAVM cards
For the first card set as primary, enter the command ptp4l -E -2 -H -i eth1 -l 6 -m -q -f ptp.cfg
For the second card set to slave, enter the command ptp4l -E -2 -H -i eth0 -s -l 6 -m -q -f ptp.cfg
The symptom is consistent with the document.
however, the slave computer fails to synchronize the host time
The test situation can be referred to the table below:
|
ptp4l tool test |
||
|
testing environment |
hardware |
software |
|
SAK-TC397AX |
V7.3.3.16.20220418 |
|
|
single-board test |
||
|
input cmd |
Board output |
problem |
|
1. ptp4l -E -2 -H -i eth0 -l 7 -m -q -p /dev/ptp0 -f ptp.cfg 2. ptp4l -E -2 -H -i eth0 -l 7 -m -q -p /dev/ptp0 |
1. ptp4l[274.850]: port 1: master tx announce timeout 2. The wireshark fails to capture packets. |
The ptp4l tool cannot output ptp packets when a single card is master |
|
Double board card test |
||
|
master:ptp4l -E -2 -H -i eth1 -l 6 -m -q -f ptp.cfg slave:ptp4l -E -2 -H -i eth0 -s -l 6 -m -q -f ptp.cfg |
The print is normal and consistent with the document description |
Query the system time. The slave board is not synchronized with the master board time |
ptp.cfg content
[global]
tx_timestamp_timeout 400