This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于OMAP-L138的超频工作的问题

Other Parts Discussed in Thread: OMAP-L138, TPS65070

大家好

        我现在的OMAP-L138是用的1.2V的内核电压工作,工作频率为300M。看了资料上说只需把1.2V的内核电压改成1.3V,就可以工作在456Mhz的频率下了,想知道还需要改变别的什么吗?

1,我供电是用TPS65070,初始上电默认的是1.2V的电压(内核),OMAPL138工作正常后,再通过IIC口改变TPS65070寄存器的值,使DCDC3输出的1.2V变成  1.3V,这样我的OMAPL138的工作频率就由300Mhz变成456Mhz了吗?

2,怎么检测频率是否升高了?用相同的一段代码测试其在不同内核电压下的运行时间可以吗?

谢谢!