This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教关于TMS320C6455自带TCP2使用问题

Other Parts Discussed in Thread: TMS320C6455

您好,我最近在使用TMS320C6455芯片自带的TCP2协处理器,目前有几个问题需要请教你们。
      我使用的是SA模式,1/2编码率,待编码信息270bits,添加CRC校验位后为294bits。编码后有588个符号和12个卷尾符号。符合3GPP2 CDMA2000。
      目前遇到的几个问题:
1、TCP2输入数据格式,我主要参考贵公司的SPRU973文档的第四章,首先关于1/2编码率的小端模式的数据格式表格是否有打印问题?其次,每个SP都是6bits,16个外部量化寄存器的量化因子是0x20,那么对于BPSK调制下(0为1,1为-1)的情况时0对应32,1对应-32。可是6个bits表示不了-32啊?这个是我那没有理解清楚?(或许1对应的是-31?)。
2、上述例程没有使用CRC校验,如果我要使用,是不是只需配置相应寄存器即可,还是还需要调用哪个函数?
3、至少使用过VCP2协处理器,记得有一个变量是用来配置编码多项式的,可是TCP2我怎么没看到有关于配置编码多项式的地方?

4、例程tcp2_standalone_mode内TCP2_statTcpState函数返回的值的含义是什么?谢谢