This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于sensor MT9P031的问题

Other Parts Discussed in Thread: PCA9306, THS7303, PCA9543A, TVP5146

请教一下关于sensor问题。

板子是DM368,用到的sensor是MT9P031,I2C电平转换用的PCA9306,平台是DVSDK4.02。

问题:PCA9306是没有器件地址的,PCA9543是有器件地址的,现在用PCA9306来替换PCA9543,是不是只需要在DVSDK里屏蔽PCA9543就可以了。

  • 如你所述的情况,应该是可以这么做

  • 多谢Eason的回答。

    下面应该是I2C设备信息,那sensor是不是也要在这添加

    static struct i2c_board_info i2c_info[] = {

     {   I2C_BOARD_INFO("dm365evm_keys", 0x25),  },  

    {   I2C_BOARD_INFO("24c256", 0x50),   .platform_data = &eeprom_info,  },

     {   I2C_BOARD_INFO("tlv320aic3x", 0x18),  },

     {   I2C_BOARD_INFO("ths7303", 0x2c),  },

     {   I2C_BOARD_INFO("PCA9543A", 0x73),  },

    };

    因为这里有注册

    static void __init evm_init_i2c(void)

     {  davinci_init_i2c(&i2c_pdata);  

    //if (have_imager())  

     //i2c_add_driver(&pca9543a_driver);

     i2c_register_board_info(1, i2c_info, ARRAY_SIZE(i2c_info));

     }

    但是为什么有些I2C设备又没添加在static struct i2c_board_info i2c_info[],比如TVP5146

    tvp5146首先是这样的

    static struct tvp514x_platform_data tvp5146_pdata =

     {        .clk_polarity = 0,        .hs_polarity = 1,        .vs_polarity = 1 };

    然后在static struct vpfe_subdev_info vpfe_sub_devs[] 中会这样,

    .board_info = {    I2C_BOARD_INFO("tvp5146", 0x5d),    .platform_data = &tvp5146_pdata,},

    这两者是不是都可以注册I2C设备

     

     

  • 此外,原本的PCA9543A的处理是这样的,

    static struct i2c_client *pca9543a;

     

    static int pca9543a_probe(struct i2c_client *client,   const struct i2c_device_id *id) {  printk("pca9543a_probe\n");  pca9543a = client;  return 0; }

     

    static int pca9543a_remove(struct i2c_client *client) {  pca9543a = NULL;  return 0; }

     

    static const struct i2c_device_id pca9543a_ids[] = {  { "PCA9543A", 0, },  { /* end of list */ }, };

     

    /* This is for i2c driver for the MT9P031 header i2c switch */ static struct i2c_driver pca9543a_driver = {  .driver.name = "PCA9543A",  .id_table = pca9543a_ids,  .probe  = pca9543a_probe,  .remove  = pca9543a_remove, };

     

    static int dm365evm_enable_pca9543a(int en) {  static char val = 1;  int status;  struct i2c_msg msg = {    .flags = 0,    .len = 1,    .buf = &val,   };

     printk("dm365evm_enable_pca9543a\n");   if (!en)   val = 0;

     if (!pca9543a)   return -ENXIO;

     msg.addr = pca9543a->addr;  /* turn i2c switch, pca9543a, on/off */  status = i2c_transfer(pca9543a->adapter, &msg, 1);  printk("dm365evm_enable_pca9543a, status = %d\n", status);   return status;  return 0; }

     

    static int dm365evm_setup_video_input(enum vpfe_subdev_id id)中

    case VPFE_SUBDEV_MT9P031:    mux |= CPLD_VIDEO_INPUT_MUX_IMAGER;    resets |= BIT(0); /* Put TVP5146 in reset */    label = "HD imager";

       dm365evm_reset_imager(1); /* Switch on pca9543a i2c switch */    if (have_imager())     dm365evm_enable_pca9543a(1);    break;

     

    static void __init evm_init_i2c(void)

     {  davinci_init_i2c(&i2c_pdata);  if (have_imager())   i2c_add_driver(&pca9543a_driver);  i2c_register_board_info(1, i2c_info, ARRAY_SIZE(i2c_info)); }