您好,我的DSP程序已通过编译生成.out文件,之后又通过ccs3.3自带的hex500.exe生成.hex文件,其中用到的.cmd文件也是参考了例程,并结合自己的工程进行了修改。
现在在ccs5000 v2.2下使用Flashburn进行Flash的烧写(flash位宽为16位)。建立.cdd文件也没问题,之后点击 Program 选 Download FBTC也显示正常连接。
之后点击Program 选 Erase Flash 进度条很快(之前有几次会持续几秒钟)。查看flash里的memory显示所有地址内都是FFFF。
再点击 Program 选 Program Flash后就出现问题了。分别有以下几种问题:
(1)进度条没有显示进度,出现提示框
Not a hex file
Use Hex Conversion Ultility
(2)进度条出现一小段,出现提示框
CHECKSUM ERROR
my cksum = aefd, flash cksum = f807
(3)出现提示框
WRITE ERROR: Attempting to write locations 0xffff8000 to 0xffff8400, which is outside the logical bounds of Flash Memory 0 to 0x40000.
这三种错误是由于所用的转换.cmd文件有所不同,相应的转换.cmd文件分别如下:
mcbsp.out /*第一个.cmd文件*/ /* Input COFF file */
-i /* Select Motorola-S1 */
-map mcbsp_hex.map /* Name hex utility map file */
-o mcbsp.hex /* Name hex output file */
-memwidth 16 /* Set EPROM system memory width */
-romwidth 16 /* Set physical ROM width */
-boot
-bootorg 0x8000
-e 80h
-swwsr 0x7fff /* Software Wait State Reg value */
-bscr 0x8806 /* Bank-Switch Control Reg */
ROMS
{
PAGE 0 : ROM : o=0x0000, l=0x10000
}
SECTIONS
{
.trap boot
.vectors boot
.stack boot
.text boot
.cinit boot
.cio boot
.switch boot
.bss boot
.const boot
.sysmem boot
}
mcbsp.out /*第二个.cmd文件*/ /* Input COFF file */
-m1 /* Select Intel format */
-map mcbsp.map
-o mcbsp.hex /* Name the hex output file */
-memwidth 16 /* Set EPROM system memory width */
-romwidth 16 /* Set physical ROM width */
-boot /* Make all sections bootable */
-bootorg 0x8000 /* Place boot table in EPROM */
-e 80h
/* starting at address 0x0000 */
ROMS
{
PAGE 0 : ROM : origin = 0x8000, length = 0x80000
}
mcbsp.out /*第三个.cmd文件*/ /* Input COFF file */
-m1 /* Select Intel format */
-map mcbsp.map
-o mcbsp.hex /* Name the hex output file */
-memwidth 16 /* Set EPROM system memory width */
-romwidth 16 /* Set physical ROM width */
-boot /* Make all sections bootable */
-bootorg 0x0000 /* Place boot table in EPROM */
-e 80h
/* starting at address 0x0000 */
ROMS
{
PAGE 0 : ROM : origin = 0x0000, length = 0x10000
}
请问我该如何解决这一问题呢?时间紧迫,希望能尽快解答我的疑惑!!!
还有,这与工程文件里面的内容有没有关系呢?比如工程链接文件link.cmd的配置???