This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am335x 双网口独立EMAC



hi guys:

        我们现在设备正在调试双网口这块,每一个EMAC对应一个ip101ah芯片,之前1口的网口已经调通。现在双网口有几个问题

1.uboot自从加了双网口之后,有些时候会不断的自动重启。硬件有些不稳定。

2.在代码修改上,

    我是分层修改的mach-omap2/devices.c 和 board-am335x-evm.c phyADDR[5] 的两个芯片值分别为1和17(也就是0:01 ,0:11)还有有关pinmux rmii2的配置

    还有就是修改了gmii_sel的值,原来是0x4D现在改为了0xC5。

3.现象,网卡eth0的连接灯是亮的,eth1连接等不亮(板子上没有设置电源灯)。

请问除了这些修改还有别的么?