This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335X USB HUB 无法识别 复位HUB方可识别 WINCE7

Other Parts Discussed in Thread: TPS2051

你好

我的AM335X核心板是在beaglebone的板子上做了删改做成的核心板,作为子板插在母板上,母板上有一颗USB2.0 HUB芯片(1转4)NEC UPD7114,之前还用过台湾安国HUB芯片的AU6258,BSP主体是335X EVM的WINCE CODE,

1,HUB芯片自供电;

2,AM335X通过的USB1与HUB芯片的上行口D+,D-直连;

3,AM335X USB1配制成HOST,限流芯片采用TPS2051,电路与beaglebone一致,未改动;

故障现象如下:

1,鼠标、键盘设别插在HUB芯片上,上电,启动系统,系统无法识别出鼠标和键盘等USB设备;

2,上电后插拔USB设备,同样无法识别设备;

3,,通过HUB芯片的RESET脚,复位HUB芯片,此时能识别出鼠标等USB设备;

4,我不能每次去复位HUB芯片,很疑惑为什么先上电HUB芯片,系统后启动,系统无法通过HUB识别出USB设备(鼠标)???是不是USB驱动的问题??经反复检查,2种HUB芯片的电路未发现问题?请问这个问题如何解决。