This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL138 NAND FLASH 烧写问题

Other Parts Discussed in Thread: OMAP-L138

你好,我想将OMAPL138的DSP核的程序加载到flash中实现程序的上电自启动,我用 NANDWriter_DSP进行烧写时程序停留在NAND_InfoHandle NAND_open(Uint32 baseCSAddr)函数的while (hNandInfo->CSOffset < DEVICE_EMIF_NUMBER_CE_REGION)循环里面,因为To generate the AIS format file, you need to run the ARM/DSP .out (COFF) file generated from CCS build through the AISGen tool.语句后面一直不能出现enter the image type 的提示字样,不知道怎么解决。