我运行TI自带的edma3数据搬移的例子, 搬移2个数组(src1,src2)到2个数组(dst1,dst2)可以成功,但当我再加一个数组,想尝试搬移三个数组(src1,2,3)到dst1,dst2,dst3,就失败了, 该怎么做
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我运行TI自带的edma3数据搬移的例子, 搬移2个数组(src1,src2)到2个数组(dst1,dst2)可以成功,但当我再加一个数组,想尝试搬移三个数组(src1,2,3)到dst1,dst2,dst3,就失败了, 该怎么做
就是TI自带的edma_test.c
myParamSetup.option = CSL_EDMA3_OPT_MAKE(CSL_EDMA3_ITCCH_DIS, \
CSL_EDMA3_TCCH_DIS, \
CSL_EDMA3_ITCINT_DIS, \
CSL_EDMA3_TCINT_EN, \
0, CSL_EDMA3_TCC_NORMAL,\
CSL_EDMA3_FIFOWIDTH_NONE, \
CSL_EDMA3_STATIC_DIS, \
CSL_EDMA3_SYNC_A, \
CSL_EDMA3_ADDRMODE_INCR, \
CSL_EDMA3_ADDRMODE_INCR );
myParamSetup.srcAddr = (Uint32)srcBuff1;
myParamSetup.aCntbCnt = CSL_EDMA3_CNT_MAKE(256,1);
myParamSetup.dstAddr = (Uint32)dstBuff1;
myParamSetup.srcDstBidx = CSL_EDMA3_BIDX_MAKE(1,1);
myParamSetup.linkBcntrld= CSL_EDMA3_LINKBCNTRLD_MAKE(hParamPong,0);
myParamSetup.srcDstCidx = CSL_EDMA3_CIDX_MAKE(0,1);
myParamSetup.cCnt = 1;
/* Ping setup */
if (CSL_edma3ParamSetup(hParamPing,&myParamSetup) != CSL_SOK)
{
printf ("Error: EDMA Parameter Entry Setup failed\n");
return -1;
};
/* Pong setup */
myParamSetup.linkBcntrld = CSL_EDMA3_LINKBCNTRLD_MAKE(hParamPing,0);
myParamSetup.option = CSL_EDMA3_OPT_MAKE(CSL_EDMA3_ITCCH_DIS, \
CSL_EDMA3_TCCH_DIS, \
CSL_EDMA3_ITCINT_DIS, \
CSL_EDMA3_TCINT_EN,\
1, CSL_EDMA3_TCC_NORMAL,\
CSL_EDMA3_FIFOWIDTH_NONE, \
CSL_EDMA3_STATIC_EN, \
CSL_EDMA3_SYNC_A, \
CSL_EDMA3_ADDRMODE_INCR, \
CSL_EDMA3_ADDRMODE_INCR );
myParamSetup.srcAddr = (Uint32)srcBuff2;
myParamSetup.dstAddr = (Uint32)dstBuff2;
if (CSL_edma3ParamSetup(hParamPong,&myParamSetup) != CSL_SOK)
{
printf ("Error: EDMA Parameter Entry Setup failed\n");
return -1;
};
/*******************************/
我加了一组类似的链接,
myParamSetup.linkBcntrld = CSL_EDMA3_LINKBCNTRLD_MAKE(hParamOut,0);
myParamSetup.option = CSL_EDMA3_OPT_MAKE(CSL_EDMA3_ITCCH_DIS, \
CSL_EDMA3_TCCH_DIS, \
CSL_EDMA3_ITCINT_DIS, \
CSL_EDMA3_TCINT_EN,\
1, CSL_EDMA3_TCC_NORMAL,\
CSL_EDMA3_FIFOWIDTH_NONE, \
CSL_EDMA3_STATIC_EN, \
CSL_EDMA3_SYNC_A, \
CSL_EDMA3_ADDRMODE_INCR, \
CSL_EDMA3_ADDRMODE_INCR );
myParamSetup.srcAddr = (Uint32)srcBuff3;
myParamSetup.dstAddr = (Uint32)dstBuff3;
if (CSL_edma3ParamSetup(hParamPong,&myParamSetup) != CSL_SOK)
{
printf ("Error: EDMA Parameter Entry Setup failed\n");
return -1;
} ;
其他的没改,前两组数据可以搬进去, 我自己加的一组就搬不过去了,是不下面的程序要改哪些参数?
/* Interrupt enable (Bits 0-1) for the global region interrupts */
regionIntr.region = CSL_EDMA3_REGION_GLOBAL;
regionIntr.intr = 0x3;
regionIntr.intrh = 0x0000;
CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTR_ENABLE,®ionIntr);
/* Trigger channel */
CSL_edma3HwChannelControl(hChannel,CSL_EDMA3_CMD_CHANNEL_SET,NULL);
regionIntr.region = CSL_EDMA3_REGION_GLOBAL;
regionIntr.intr = 0;
regionIntr.intrh = 0;
/* Poll on IPR bit 0 */
do {
CSL_edma3GetHwStatus(hModule,CSL_EDMA3_QUERY_INTRPEND,®ionIntr);
} while (!(regionIntr.intr & 0x1));
/* Clear the pending bit */
CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTRPEND_CLEAR,®ionIntr);
/* Trigger Channel */
CSL_edma3HwChannelControl(hChannel,CSL_EDMA3_CMD_CHANNEL_SET,NULL);
/* Poll on IPR bit 2 */
do {
CSL_edma3GetHwStatus(hModule,CSL_EDMA3_QUERY_INTRPEND,®ionIntr);
} while (!(regionIntr.intr & 0x2));
/* Check transfer by comparing the source and destination buffers */
if(Verify_Transfer( 256, 1, 1, 0, 0, 0, 0, srcBuff1, dstBuff1, TRUE) == FALSE)
{
printf ("Error: Verification (Source1/Destination1) Failed\n");
return -1;
}
if(Verify_Transfer( 256, 1, 1, 0, 0, 0, 0, srcBuff2, dstBuff2, TRUE) == FALSE)
{
printf ("Error: Verification (Source2/Destination2) Failed\n");
return -1;
}
/* Close channel */
if (CSL_edma3ChannelClose(hChannel) != CSL_SOK)
{
printf("Error: EDMA Channel Close failed\n");
return -1;
}
/* Close EDMA module */
if (CSL_edma3Close(hModule) != CSL_SOK)
{
printf("Error: EDMA Module Close failed\n");
return -1;
};
直接copy过来看着有点乱 麻烦了
hParamOut 是我自己定义的
hParamOut = CSL_edma3GetParamHandle(hChannel,3,&status);
EDMA有3个要素:
1. 触发方式,event 触发/手动触发/event chain式触发
2. PaRAM配置
3. 触发使能和提交
1.看你的代码你应该用的是手动触发,你要确认你新增的触发源是否和以前的有冲突;
2. 新增触发源对应的PaRAM选择是否正确
3. PaRAM的配置中,参数是否正确,例如使用全局地址
4. 判断传输完成的event 设置是否正确,例如TCC的配置是否有冲突
我新增的触发源和参数配置都是没问题的,TCC是否有冲突是怎么看的?后面这三个函数调用机制我不太懂,搬移2组他调用2次,我搬移三组是否就调用三次?
regionIntr.region = CSL_EDMA3_REGION_GLOBAL;
regionIntr.intr = 0x7;
regionIntr.intrh = 0x0000;
CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTR_ENABLE,®ionIntr);
/* Trigger channel */
CSL_edma3HwChannelControl(hChannel,CSL_EDMA3_CMD_CHANNEL_SET,NULL);
CSL_edma3GetHwStatus(hModule,CSL_EDMA3_QUERY_INTRPEND,®ionIntr);
1.红色的部分就是用来配TCC number的,你用的是1和第二个配置相同
myParamSetup.option = CSL_EDMA3_OPT_MAKE(CSL_EDMA3_ITCCH_DIS, \
CSL_EDMA3_TCCH_DIS, \
CSL_EDMA3_ITCINT_DIS, \
CSL_EDMA3_TCINT_EN,\
1, CSL_EDMA3_TCC_NORMAL,\
CSL_EDMA3_FIFOWIDTH_NONE, \
CSL_EDMA3_STATIC_EN, \
CSL_EDMA3_SYNC_A, \
CSL_EDMA3_ADDRMODE_INCR, \
CSL_EDMA3_ADDRMODE_INCR );
2.
regionIntr.region = CSL_EDMA3_REGION_GLOBAL;
regionIntr.intr = 0x7;
regionIntr.intrh = 0x0000;
CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTR_ENABLE,®ionIntr);
用来选择使用哪个shadow region和对应region中断event的使能,EDMA总共有8个Shadow region和1个global region
/* Trigger channel */
CSL_edma3HwChannelControl(hChannel,CSL_EDMA3_CMD_CHANNEL_SET,NULL);
用来手动触发EDMA 传输
CSL_edma3GetHwStatus(hModule,CSL_EDMA3_QUERY_INTRPEND,®ionIntr);
用来等待传输是否完成,对应的TPCC_IPR 中断标志是否被置位
谢谢你 将的很清楚 不过我改了TCC还是跑不了 另外我不知道我的regionintr配置是否正确 麻烦你帮我看下。
int EdmaTrans ()
{
CSL_Edma3Handle hModule;
CSL_Edma3Obj edmaObj;
CSL_Edma3ParamHandle hParamPing;
CSL_Edma3ParamHandle hParamPong;
CSL_Edma3ParamHandle hParamOut;
CSL_Edma3ChannelObj chObj;
CSL_Edma3CmdIntr regionIntr;
CSL_Edma3ChannelHandle hChannel;
CSL_Edma3ParamSetup myParamSetup;
CSL_Edma3Context context;
CSL_Edma3ChannelAttr chAttr;
CSL_Status status;
int instNum;
unsigned char channelNum;
instNum = 1;
channelNum = 1;
/* Module initialization */
if (CSL_edma3Init(&context) != CSL_SOK)
{
printf ("Error: EDMA module initialization failed\n");
return -1;
}
/* Open the EDMA Module using the provided instance number */
hModule = CSL_edma3Open(&edmaObj, instNum, NULL, &status);
if ( (hModule == NULL) || (status != CSL_SOK))
{
printf ("Error: EDMA module open failed\n");
return -1;
}
/* Channel open */
chAttr.regionNum = CSL_EDMA3_REGION_GLOBAL;
chAttr.chaNum = channelNum;
hChannel = CSL_edma3ChannelOpen(&chObj, instNum, &chAttr, &status);
if ((hChannel == NULL) || (status != CSL_SOK))
{
printf ("Error: Unable to open EDMA Channel:%d\n", channelNum);
return -1;
}
if(!instNum)
{
/* For first EDMA instance there are only 2 TCs and 2 event queues
* Modify the channel default queue setup from 0 to 1
*/
if (CSL_edma3HwChannelSetupQue(hChannel,CSL_EDMA3_QUE_1) != CSL_SOK)
{
printf ("Error: EDMA channel setup queue failed\n");
return -1;
}
}
else
{
/* For EDMA instance 1 and 2 maximum of 4 TCs and 4 event queues are supported
* Change Channel Default queue setup from 0 to 3
*/
if (CSL_edma3HwChannelSetupQue(hChannel,CSL_EDMA3_QUE_3) != CSL_SOK)
{
printf ("Error: EDMA channel setup queue failed\n");
return -1;
}
}
CSL_edma3MapDMAChannelToParamBlock (hModule, channelNum, 2);
hParamPing = CSL_edma3GetParamHandle(hChannel, 2, &status);
/* Obtain a handle to parameter set 1 */
hParamPong = CSL_edma3GetParamHandle(hChannel, 1, &status);
hParamOut = CSL_edma3GetParamHandle(hChannel,3,&status);
/* Setup the parameter entry parameters (Ping buffer) */
myParamSetup.option = CSL_EDMA3_OPT_MAKE(CSL_EDMA3_ITCCH_DIS,
CSL_EDMA3_TCCH_DIS,
CSL_EDMA3_ITCINT_DIS,
CSL_EDMA3_TCINT_EN,
0, CSL_EDMA3_TCC_NORMAL,
CSL_EDMA3_FIFOWIDTH_NONE,
CSL_EDMA3_STATIC_DIS,
CSL_EDMA3_SYNC_A,
CSL_EDMA3_ADDRMODE_INCR,
CSL_EDMA3_ADDRMODE_INCR );
myParamSetup.srcAddr = (Uint32)srcBuff1;
myParamSetup.aCntbCnt = CSL_EDMA3_CNT_MAKE(15,1);
myParamSetup.dstAddr = (Uint32) dstBuff1;
myParamSetup.srcDstBidx = CSL_EDMA3_BIDX_MAKE(0,0);
myParamSetup.linkBcntrld= CSL_EDMA3_LINKBCNTRLD_MAKE(hParamPong,0);
myParamSetup.srcDstCidx = CSL_EDMA3_CIDX_MAKE(0,0);
myParamSetup.cCnt = 1;
/* Ping setup */
if (CSL_edma3ParamSetup(hParamPing,&myParamSetup) != CSL_SOK)
{
printf ("Error: EDMA Parameter Entry Setup failed\n");
return -1;
}
/* Pong setup */
myParamSetup.option = CSL_EDMA3_OPT_MAKE(CSL_EDMA3_ITCCH_DIS,
CSL_EDMA3_TCCH_DIS,
CSL_EDMA3_ITCINT_DIS,
CSL_EDMA3_TCINT_EN,
1, CSL_EDMA3_TCC_NORMAL,
CSL_EDMA3_FIFOWIDTH_NONE,
CSL_EDMA3_STATIC_DIS,
CSL_EDMA3_SYNC_A,
CSL_EDMA3_ADDRMODE_INCR,
CSL_EDMA3_ADDRMODE_INCR );
myParamSetup.srcAddr = (Uint32)srcBuff2;
myParamSetup.aCntbCnt = CSL_EDMA3_CNT_MAKE(15,1);
myParamSetup.dstAddr = (Uint32)dstBuff2;
myParamSetup.srcDstBidx = CSL_EDMA3_BIDX_MAKE(1,0);
myParamSetup.linkBcntrld = CSL_EDMA3_LINKBCNTRLD_MAKE(hParamPing,0);
myParamSetup.srcDstCidx = CSL_EDMA3_CIDX_MAKE(0,0);
myParamSetup.cCnt = 1;
if (CSL_edma3ParamSetup(hParamPong,&myParamSetup) != CSL_SOK)
{
printf ("Error: EDMA Parameter Entry Setup failed\n");
return -1;
}
myParamSetup.option = CSL_EDMA3_OPT_MAKE(CSL_EDMA3_ITCCH_DIS,
CSL_EDMA3_TCCH_DIS,
CSL_EDMA3_ITCINT_DIS,
CSL_EDMA3_TCINT_EN,
2, CSL_EDMA3_TCC_NORMAL,
CSL_EDMA3_FIFOWIDTH_NONE,
CSL_EDMA3_STATIC_DIS,
CSL_EDMA3_SYNC_A,
CSL_EDMA3_ADDRMODE_INCR,
CSL_EDMA3_ADDRMODE_INCR );
myParamSetup.srcAddr = (Uint32)srcBuff3;
myParamSetup.dstAddr = (Uint32) dstBuff3;
myParamSetup.linkBcntrld = CSL_EDMA3_LINKBCNTRLD_MAKE(hParamOut,0);
CSL_edma3ParamSetup(hParamOut,&myParamSetup);
regionIntr.region = CSL_EDMA3_REGION_GLOBAL;
regionIntr.intr = 0x7;
regionIntr.intrh = 0x0000;
CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTR_ENABLE,®ionIntr);
CSL_edma3HwChannelControl(hChannel,CSL_EDMA3_CMD_CHANNEL_SET,NULL);
CSL_edma3GetHwStatus(hModule,CSL_EDMA3_QUERY_INTRPEND,®ionIntr);
/* Interrupt enable (Bits 0-1) for the global region interrupts */
regionIntr.region = CSL_EDMA3_REGION_GLOBAL;
regionIntr.intr = 0x3;
regionIntr.intrh = 0x0000;
CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTR_ENABLE,®ionIntr);
/* Trigger channel */
CSL_edma3HwChannelControl(hChannel,CSL_EDMA3_CMD_CHANNEL_SET,NULL);
regionIntr.region = CSL_EDMA3_REGION_GLOBAL;
regionIntr.intr = 0;
regionIntr.intrh = 0;
CSL_edma3GetHwStatus(hModule,CSL_EDMA3_QUERY_INTRPEND,®ionIntr);
/* Clear the pending bit */
CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTRPEND_CLEAR,®ionIntr);
/* Trigger Channel */
CSL_edma3HwChannelControl(hChannel,CSL_EDMA3_CMD_CHANNEL_SET,NULL);
/* Poll on IPR bit 2 */
CSL_edma3GetHwStatus(hModule,CSL_EDMA3_QUERY_INTRPEND,®ionIntr);
if (CSL_edma3ChannelClose(hChannel) != CSL_SOK)
{
printf("Error: EDMA Channel Close failed\n");
return -1;
}
if (CSL_edma3Close(hModule) != CSL_SOK)
{
printf("Error: EDMA Module Close failed\n");
return -1;
}
return 0;
}
其实我做的是TCP3E一个传输的任务,只要简单的完成TCP3E传输功能 ,不使用BIOS 他的EDMA3需要传输 配置信息和输入数据进入TCP3E,然后传输turbo encoder后的结果出来 ,所以我感觉edma3 需要三次传输。
建议不要直接增加代码,你先理解清楚样例中的实现是如何对EDMA进行操作的,之后再按照你的需求进行修改。