我使用的u-boot是开发包自带的uboot_NAND_DM816X_EVM,我按照DM8168_DVR_RDK_Install_Duide.pdf向NAND中flash内核和文件系统,设置好启动变量并使用saveenv保存这些变量后,使用命令boot可以正常启动,但是当我重启板子后却无法启动,显示如下错误:
Card did not respond to voltage select!
** Can't read from device 0 **
** Unable to use mmc 0:1 for fatload **
我用printenv命令,发现修改的变量全都没有保存
当我重新设置启动变量后,然后boot就可以启动了,这是什么原因啊?