This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL138 内部寄存器无法访问,求解?急急急



我们的单板沿了OMAPL138 EVM的多数硬件设计,并在其中外扩一个CPLD挂在EMA—CS3上,相应的PINMUX都已经配置,从PINMUX能够读取总线已经配置成AEMIF。

但是,在驱动中用ioremap(0x6200 0000, 0x1000)后(映射返回地址均是 0xC000 0000 0xDFFF FFFF区间内),但仍然无法进行读取,我们通过示波器测量过EMA_CLK是有100MHZ的时钟输入,可就是没有CS3的片选信号,请问高手,此处是什么原因?

如下是EMIFA相关的物理地址,我都经过ioremap的测试,都没有CS信号,也不能正常读取。但是其它ARM内部寄存器可以,比如UART0,1,2,  timer1,2,。

 0x4000 0000 0x5FFF FFFF 512M EMIFA SDRAM data (CS0)
0x6000 0000 0x61FF FFFF 32M EMIFA async data (CS2)
0x6200 0000 0x63FF FFFF 32M EMIFA async data (CS3)
0x6400 0000 0x65FF FFFF 32M EMIFA async data (CS4)
0x6600 0000 0x67FF FFFF 32M EMIFA async data (CS5)
0x6800 0000 0x6800 7FFF 32K EMIFA Control Regs