This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm8127 rdk3.2 FVID2结构体



大家好,

在各个link之间传递frame的结构为FVID2_Frame;在addr单元中存放的为Y UV分量的地址;

    请问:各个link阶段的YUV组织形式是什么(YUV420 YUV444等)?如何对Y UV分量进行操作?一帧图像的空间在哪里分配的?哪里有相关文档可以参考?

谢谢

  • 你好,

       请参考结构体定义以及注释,路径\ti_tools\hdvpss\dvr_rdk_hdvpss\packages\ti\psp\vps\fvid2.h

    typedef struct
    {
    Ptr addr[FVID2_MAX_FIELDS][FVID2_MAX_PLANES];
    /**<
    FVID2 buffer pointers for supporting multiple addresses like
    Y, U, V etc for a given frame. The interpretation of these pointers
    depend on the format configured for the driver.
    The first dimension represents the field and the second dimension
    represents the color plane.
    Not all pointers are valid for a given format.

    Representation of YUV422 Planar Buffer:
    Field 0 Y -> addr[0][0], Field 1 Y -> addr[1][0]
    Field 0 U -> addr[0][1], Field 1 U -> addr[1][1]
    Field 0 V -> addr[0][2], Field 1 V -> addr[1][2]
    Other pointers are not valid.

    Representation of YUV422 Interleaved Buffer:
    Field 0 YUV -> addr[0][0], Field 1 YUV -> addr[1][0]
    Other pointers are not valid.

    Representation of YUV420SP or YUV422SP Buffer:
    Field 0 Y -> addr[0][0], Field 1 Y -> addr[1][0]
    Field 0 UV -> addr[0][1], Field 1 UV -> addr[1][1]
    Other pointers are not valid.

    Representation of RGB888 Buffer
    Field 0 RGB -> addr[0][0], Field 1 RGB -> addr[1][0],
    Other pointers are not valid.

    For progressive mode data formats
    or when fields are processed by driver in frame mode.
    addr[1][x] is not used.

    Instead of using numerical for accessing the buffers, the application
    can use the macros defined for each buffer formats like
    FVID2_YUV_INT_ADDR_IDX, FVID2_RGB_ADDR_IDX, FVID2_FID_TOP etc. */

    UInt32 fid;
    /**< Indicates whether this frame belong to top or bottom field.
    For valid values see #FVID2_Fid. */
    UInt32 channelNum;
    /**< Channel number to which this FVID2 frame belongs to. */

    UInt32 timeStamp;
    /**< Time stamp returned by the driver, in units of msecs.
    Only valid for frames received using FVID2_dequeue(). */
    Ptr appData;
    /**< Additional application parameter per frame. This is not modified by
    driver. */

    Ptr perFrameCfg;
    /**< Per frame configuration parameters like scaling ratio, positioning,
    cropping etc...
    This should be set to NULL if not used.

    This can be used by application to control driver behaviour on a per
    frame basis, example changing scaling ratio for scalar driver.

    This can be used by application to get per frame status, example
    detected frame width, height from capture driver.

    This could be set to NULL if not used. In this case, the driver will
    use the last supplied configuration.

    The exact structure type that is passed is driver specific. */

    Ptr blankData;
    /**< Blanking data associated with this video frame.
    This could be set to NULL if not used. */

    Ptr drvData;
    /**< Used by driver. Application should not modify this. */

    FVID2_SubFrameInfo *subFrameInfo;
    /**< Used for SubFrame level processing information exchange between
    application and driver.
    This could be set to NULL if sub-frame level processing is not used. */

    Ptr reserved;
    /**< For future use. Not used currently. Set this to NULL. */

    } FVID2_Frame;

  • 谢谢您的支持!

    看过之后还是有两点不清楚:

    1 addr[][]中存放的是Y U V分量的指针,我想知道指向的内容在哪里分配的?

    2 哪里指定Y U V的数据格式?如是444还是420等?

    谢谢!