This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678+ARM视频采集系统中ARM的选择



我拟采用C6678+ARM实现视频采集编码功能,请问ARM采用什么型号好?请各位专家给我一些建议。谢谢!

  • 你们的系统ARM主要功能是什么,一般来说ARM主要做系统控制,做人机界面,DSP加载,系统操作维护等功能,这部分功能TI的AM335x系列有很多成熟的产品可供选择。另外要考虑ARM和DSP之间的数据接口,是否有海量数据传输从而选定相关外设做设计。

  • 你好,

    如果你的视频输入是单路CMOS/CCD的camera,而且需要h264编码,你可以考虑DM8127.

    如果你的视频输入是多路标清,高清视频,需要编解码,可以考虑DM816x, DM814x。

    上面的DM产品都可以通过PCIe和C66芯片连接。