您好:
我的芯片上写的型号如下:
TMS320
C6748BZCE E
23A3J3W GI A375
21 527 ZCE
请问,第二排的单独的E 是指增强型?还是加密?这类芯片在连接JTAG的时候有什么特殊要求吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好:
我的芯片上写的型号如下:
TMS320
C6748BZCE E
23A3J3W GI A375
21 527 ZCE
请问,第二排的单独的E 是指增强型?还是加密?这类芯片在连接JTAG的时候有什么特殊要求吗
一般是不建议在加密芯片上来调试,都是在普通芯片上调成好以后,将生成的可执行文件转换为加密芯片使用的可执行文件。
在连接中有描述:
Application development and debugging on a secure device is not really recommended but there is flexibility in the boot process that allow this functionality when required. The ini file for creation of secure boot images contains field called BootExitType and TAPCFG. Specifying the BootExit type as NONSECURE and TAPCFG= 0x0000FFFF will force the device to exit ROM boot in NON-secure mode and open the JTAG pins to connect the emulator.