This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm368 gadget驱动报错



大家好,我在使用ipnc_rdk5.0的时候遇到问题,1:将usb驱动配置成otg或者peripheral,加载g_ether.ko模块,报如下错误:

[  151.243834] g_ether gadget: using random self ethernet address
[  151.249730] g_ether gadget: using random host ethernet address
[  151.258103] usb0: MAC f2:dc:82:e8:98:d2
[  151.262764] usb0: HOST MAC 36:4c:bd:7f:b0:2e
[  151.267178] g_ether gadget: Ethernet Gadget, version: Memorial Day 2008
[  151.274876] g_ether gadget: g_ether ready
root@192:/opt/ipnc/modules# [  151.515257] usb connect
[  153.934760] usb connect
[  153.937355] ------------[ cut here ]------------
[  153.941993] WARNING: at fs/proc/generic.c:589 0xc00e46b4()
[  153.947484] proc_dir_entry '/proc/usb_connect' already registered
[  153.953575] Modules linked in: g_ether davinci nop_usb_xceiv ppp_deflate ppp_generic netconsole slhc tun loop cppi_dma musb_hdrc iscsi_tcp libiscsi_tcp libiscsi scsi_transport_iscsi davinci_mmc mmc_block mmc_core libcrc32c sha1_generic md5 des_generic crc32c crc_ccitt
[  153.977497] Backtrace:
[  153.979958] Function entered at [<c002c4ec>] from [<c02ba83c>]

每加载一次模块,在/proc下就会生成三个usb_connect的节点,卸载模块后节点也不消失,在pc端能识别到网卡,但是配置ip后不能ping通,请问这是什么原因?困惑了很久了,希望ti的专家们能帮忙解答一下,谢谢!附件是内核配置文件