This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm368 madplay播放无声音



ti的专家你们好,我在使用ipnc_rdk5.0的时候遇到一些问题:1:使用移植后的madplay 播放mp3,程序运行正常,

MPEG Audio Decoder 0.15.2 (beta) - Copyright (C) 2000-2004 Robert Leslie et al.
          Title: ····
         Artist: ···
          Album: ····
           Year: 1989
 00:05:00 Layer III, 128 kbps, 44100 Hz, single channel, no CRC
11485 frames decoded (0:05:00.0), +0.6 dB peak amplitude, 66 clipped samples,

但是喇叭上没有声音,cpu引脚上也无波形,换成ipnc_rdk3.1后就能正常播放,也有声音,我在驱动配置里也选择了兼容oss,请问这是什么原因造成的?

2:rtc的驱动只能配置成模块,编译进内核会导致i2c总线不能使用,这个问题很匪夷所思,不知道什么原因,不过这并不影响使用。没有查到有用的资料,只能来这里求助,希望你们能帮忙解答,谢谢!