This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于6678的timer64看门狗的问题



打算使用6678的timer64看门狗功能,初始化之后等待看门狗超时,检查WDFLAG标志,确实已经置位,但芯片似乎没有复位,代码还在正常运行。

想请问一下:

6678的timer64看门狗功能可以复位整个芯片么,如果可以,应该怎么设置?

  • 可以复位整个芯片,需要配置RSTMUX register,配置watchdog timer output mode,该寄存器的定义见C6678 data manual,可以参考如下STK Robust例程中的watchdog test配置。

    http://www.deyisupport.com/question_answer/dsp_arm/c6000_multicore/f/53/t/47664.aspx