This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

新手关于NDK2.0使用的问题



您好!

       我的开发板是OMAPL137的DSP,最近在使用NDK实现PC机与DSP的通信,但是在运行NDK的列子client时,出现以下情况:

       TCP/IP Stack Example Client Using MAC Address: f0-0f-f0-0f-f0-0f  

      EMAC should be up and running 

      EMAC has been started successfully

     Registeration of the EMAC Successful

     Service Status: DHCPC    : Enabled  :          : 000

     Service Status: Telnet   : Enabled  :          : 000

     Service Status: HTTP     : Enabled  :          : 000

     Service Status: DHCPC    : Enabled  : Running  : 000

     Link Status: 100Mb/s Full Duplex on PHY 0

    Service Status: DHCPC    : Enabled  : Fault    : 002

    Service Status: DHCPC    : Disabled :          : 000

    Service Status: DHCPC    : Enabled  :          : 000

    Service Status: DHCPC    : Enabled  : Running  : 000

   没有出现所谓的IP地址和其他信息,希望哪位高手能帮助解答,不甚感激!

   谢谢您的回答!