This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问ti达芬奇系列芯片中有没有支持bt1120格式的复合流的10比特高清输入的?



如题,bt1120格式的高清流分为两种,一种是Y datastream 和 Cb/Cr datastream,分开的两个流,20比特接收。另一种是multiplexed parallel data stream,10比特接收,请问,有没有直接支持10比特接收bt1120格式复合流的芯片,达芬奇64系列中是否有支持10比特接收bt1120格式复合流的芯片?

接收bt1120格式Y datastream 和 Cb/Cr datastream的两个流,20比特接收的芯片有木有?

  • 据我所知,应该木有支持20bit BT1120的,DM81xx 支持BT1120,8bit或者16bit Y/Cb/Cr采集。

    Each video input capture port can be operated as one 16-bit input channel (with separate Y and Cb/Cr inputs) or two clock independent 8-bit input channels (with interleaved Y/C data input). Further one of the VIP ports can operate in 24-bit mode to support RGB capture.