This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

8168 nfs只能dhcp方式挂载



我用8168做的板子 uboot以tftp方式载入kernel,bootargs配置以nfs方式挂载文件系统,bootargs中ip设置为dhcp能正常挂载文件系统,指定ip则报错,bootargs 具体设定为:  bootargs 'mem=128M console=ttyO2,115200n8 rw ip=192.168.1.9:192.168.1.100:192.168.1.100:255.255.255.0::eth0:off root=/dev/nfs rootfstype=jffs2 nfsroot=192.168.1.100:/home/ti/netra/target/rfs eth=00:0C:29:94:D7:D6 vram=20M notifyk.vpssm3_sva=0xBFD00000'  ,kernel打印报错信息为:

..............
davinci_mdio davinci_mdio.0: resetting idled controller
net eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:00, id=221612)
IP-Config: Complete:
     device=eth0, addr=192.168.1.9, mask=255.255.255.0, gw=192.168.1.100,
     host=192.168.1.9, domain=, nis-domain=(none),
     bootserver=192.168.1.100, rootserver=192.168.1.100, rootpath=
VFS: Unable to mount root fs via NFS, trying floppy.
List of all partitions:
1f00            2304 mtdblock0  (driver?)
1f01             256 mtdblock1  (driver?)
1f02            4352 mtdblock2  (driver?)
1f03          255232 mtdblock3  (driver?)
No filesystem could mount root, tried:  jffs2
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)
Backtrace:
[<c0045b7c>] (dump_backtrace+0x0/0x110) from [<c0352404>] (dump_stack+0x18/0x1c)
 r7:c6413000 r6:c0068c28 r5:c002b5dc r4:c04b6fd0
[<c03523ec>] (dump_stack+0x0/0x1c) from [<c0352468>] (panic+0x60/0x17c)
[<c0352408>] (panic+0x0/0x17c) from [<c0009254>] (mount_block_root+0x1e0/0x220)
 r3:00000000 r2:00000020 r1:c6423f58 r0:c03fe41c
[<c0009074>] (mount_block_root+0x0/0x220) from [<c0009340>] (mount_root+0xac/0xcc)
[<c0009294>] (mount_root+0x0/0xcc) from [<c00094d0>] (prepare_namespace+0x170/0x1d4)
 r4:c04b6924
[<c0009360>] (prepare_namespace+0x0/0x1d4) from [<c0008784>] (kernel_init+0x114/0x154)
 r5:c0008670 r4:c04b68c0
[<c0008670>] (kernel_init+0x0/0x154) from [<c0068c28>] (do_exit+0x0/0x5e4)
 r5:c0008670 r4:00000000

确定pc端nfs服务是正常的,因为dhcp方式能挂载,kernel中也确保nfs选项都已经选中,不知道大家有没有碰到类似问题,还望各位高手不吝赐教