This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

源码从6670迁移到6614

Other Parts Discussed in Thread: SYSBIOS

Hi:

    我们原是基于C6670芯片开发代码,使用的CCS版本使5.1.09,由于工作需要,现在要将代码移植到C6614上去,使用的CCS版本是5.5,遇到了如下图所示的一个问题,请各位大侠帮忙看一下:

另外,请问是否有从6670迁移代码6614的手册,或者类似的资料。谢谢!

  • 6670与6614代码时完全兼容的,只需替换CSL,可能某些宏定义不一致。

    从出错来看像是sysBios版本的问题,6670的工程在CCS5.5下能编译成功么?

  • 6670的工程在ccs5.5上只需要做简单的修改就可以编译通过,但是使用6614的就不行,图中遇到的问题该怎么解决呢?

  • 从6670到6614移植你做了哪些修改?

    从错误现象来看感觉是sysBios版本问题,与6670及6614没有关系,应该在6670编译也会有相同的问题出现。

  • Andy,谢谢您的回答。我们从6670到6614做了如下修改:1 将Build_Profile的有whole_Program修改为release;

                                                                                                            2 将pdk由6670换成了6614的PDK;

                                                                                                            3  Sys/bios版本,XDC版本,EDMA的版本都修改成了最新的;

  • 1 将Build_Profile的有whole_Program修改为release;

    2 将pdk由6670换成了6614的PDK;

    3  Sys/bios版本,XDC版本,EDMA的版本都修改成了最新的;

    如上修改,从6670到6614,如果只修改第二点PDK,会出现问题么?在c6670下,如果修改1,3应该也会出问题吧?

    上面你报的问题我觉得是sysios、xdc版本问题,可以试试只改1,2试试。

  • Andy谢谢您的帮助,我查阅了一些BIOS的手册,发现XDC和BIOS版本不对应的,会造成这个错误。谢谢您的帮忙。

  • 你好,我有个6670的问题,能留一个联系方式吗?方便交流