dear all,
我一直想知道DM385和8127中的两个cortexM3的主频是多少,因为现在打算在VIDEO M3和VPSS M3中做一些算法,却并不知道大的方面可否行的通,有谁知道的么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
dear all,
我一直想知道DM385和8127中的两个cortexM3的主频是多少,因为现在打算在VIDEO M3和VPSS M3中做一些算法,却并不知道大的方面可否行的通,有谁知道的么?
1. 芯片是有不同速度等级的版本的。
2. 最高速的版本,M3可以跑到280MHz
3. 不知道你说的算法有多复杂。实现是可以的。
我想利用capture一路D1的小码流,然后再VPSSM3中做一个帧间差分算法来做移动侦测。
从DM36X就做过来,发现自带的那个MV算法很不好用,所以计划重新实现。
我们现在使用的是APPRO发布的最新的DM388+IM185的方案,这个的VPSS M3可以跑到280MHZ么?如果能跑到那肯定就够用了
我知道了,我这M3的主频是200MHZ,有点低了,这样的话需要把这个算法想办法移动到A8中去做。
尽量就A8吧,编程应该也容易点。
M3怎么说都是个单片机的内核