我们目前正在dm368平台做开发,dvsd4.0.2开发包,mt9p031数据输入图像正常,现在我们用黑白的sensor输入数据,不能显示正常的图像,能够产生场信号的中断,想问一下各位黑白的数据输入对dm368的处理有没有什么影响?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们目前正在dm368平台做开发,dvsd4.0.2开发包,mt9p031数据输入图像正常,现在我们用黑白的sensor输入数据,不能显示正常的图像,能够产生场信号的中断,想问一下各位黑白的数据输入对dm368的处理有没有什么影响?
你好,
请问黑白的sensor在分辨率上和9P031是否一致,不一致的话是否修改了相应的参数?
DM36x的ISIF是不知道输入的sensor是黑白还是彩色的。但如果是彩色的RAW,是需要经过IPIPE转换为YUV输出的。我理解黑白的sensor应该不需要在过IPIPE做插值了吧。如果是,请尝试让RAW在ISIF的输出到DDR,看数据是否正常。
您好,
你说的很有道理,把ipip里面的RAW数据转换YUVdisable了,那preview这个功能也没了吧?RAW不能直接preview的。我现在用的开发包是dvsd4.0.2,对于获取Raw数据有点迷茫,能指导一下吗?或者有什么关于dvsd4.02的文档给我看一下。