This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] 关于boot的总结

Other Parts Discussed in Thread: CCSTUDIO, OMAP-L138, SYSBIOS

本人总结了关于TI DSP的boot原理,格式,以及参考代码供大家参考。不足之处,敬请指正。

2014.12.8: 更新:改成CCSV5.5工程,内容稍做修改与简化。

也可以参考Starterware里的bootloader example,说明如下:

C6748 StarterWare Booting And Flashing

Contents

The StarterWare Bootloader[edit]

The StarterWare bootloader is a platform-specific helper application that makes it easy to transition from running a StarterWare application in a debug context (i.e. in Code Composer Studio with a GEL file) to a production context (i.e. running the application automatically when the board is powered on). The bootloader acts as an intermediary between the ROM bootloader (RBL) and the application. During boot, the StarterWare bootloader takes the following actions:

  1. Applies common PLL and DDR/EMIF settings
  2. Copies application program and data sections from flash memory to DDR
  3. Jumps to application entrypoint

If the bootloader encounters an error during boot, it prints diagnostic messages to the UART console.

The StarterWare bootloader comes pre-built with the standard installation and typically does not need to be modified or rebuilt unless you want to port it to a custom hardware platform. The prebuilt binary can be found in the following location:

<StarterWare Installation Path>/binary/armv5/<toolchain>/c6748/evmC6748/bootloader/Release/boot.out

Booting a StarterWare Application[edit]

Binary Image Generation[edit]

Booting a StarterWare application requires two binary images:

  1. An AIS file containing the StarterWare bootloader
  2. A binary file containing the application

These images are generated using two separate tools, both of which are included in the tools folder of the standard StarterWare installation.

Using AISgen to Create the Bootloader AIS File[edit]

The AISgen GUI can be used to generate the StarterWare bootloader AIS file. All of the critical settings are located on the General tab of the AISgen GUI:

  • Boot Mode - Set to SPI0 Flash
  • Application File - Set to bootloader .out file
  • AIS Output File - Desired AIS file name/path

The AISgen tool has many options to configure the device at boot time, but these are generally not necessary since the StarterWare bootloader will boot very quickly and apply its own configuration immediately. The following screenshot shows the typical settings that should be specified to generate the bootloader AIS file. Simply click the Generate AIS button to create the AIS file.

NOTE
You will typically need to generate the bootloader AIS file only once. That same AIS file can be used with any number of different applications.

Using out2rprc to Create the Application Binary[edit]

The out2rprc command line utility is used to generate the application binary image. This tool strips out the initialized sections from the executable file (i.e. *.out) and places them in a compact format that the StarterWare bootloader can understand. Generating this binary file is very simple:

$> out2rprc.exe [application].out [application].bin

The output (bin) file is typically much smaller than the original executable (out) file.

Flashing the Application[edit]

Once you have generated both binary images (i.e. the AIS and bin files described above), you are ready to flash these images to the EVM's SPI flash memory. This can be done using the standard serial flasher utility that's included in the tools folder of the standard StarterWare installation:

  1. Set the boot switches for UART2 boot (5:8 = 0011 on EVM)
  2. Run SFH from the command line:
    • $> sfh_OMAP-L138.exe -flash -targetType C6748 [bootloader].ais [application].bin
  3. Power on or reset the EVM

The SFH tool may take several minutes to complete depending on the size of the application. When SFH completes successfully, your application is ready to boot.

NOTE
The SFH tool automatically adds simple header information to the application binary file. This header tells the bootloader basic information about the application contents, including its total size in bytes.

Booting the Application[edit]

After the binary images have been flashed to the EVM, the application is ready to boot. This is as simple as setting the boot switches for SPI0 flash boot (5:8 = 0000 on the EVM) and powering on or resetting the board.

During boot, control passes from the ROM bootloader to the StarterWare bootloader, which configures the system and loads the application. Finally, the bootloader jumps to the application entrypoint. The overall process is summarized in the following diagram.

Boot_DSP_on_SOC_V0.2.zip
  • 这个应该加精. :)

  • Tony您好,我看了这个Boot_DSP_on_SOC_V0.1,我尝试在仿真器上首先执行arm程序,然后loaddsp到RAM上,随后使用唤醒操作dsp,但是,发现唤醒后,dsp并没有执行(led没有变化),

    为验证程序争取与否,我尝试单独用仿真器加载这个dsp文件测试可以正常工作,如点亮led.这是为什么呢?

  • 可以先把DSP RESET 一下

    在

    //Wake up the DSP前面加上

    CSL_FINST(psc0Regs->MDCTL[CSL_PSC_DSP], PSC_MDCTL_LRST, ASSERT);

    while(CSL_FEXT(psc0Regs->PTSTAT, PSC_PTSTAT_GOSTAT1)==CSL_PSC_PTSTAT_GOSTAT1_IN_TRANSITION);

  • Tony您好:

     我看了您写的 Boot_DSP_on_SOC_V0.1,所以想尝试一个在用CCS跑一下您的ARM程序(OMAPL138_ARMbootDSPCoff\OMAPL138DemoInterrupt),但打开后发现没有.pjt文件(可能是我知道的太少了),所以就用OMAPL138DemoInterrupt中的代码自己建了一个工程,同时又手动添加了rts67plus.lib,编译链接时出现了下面的错误。

    error: library 'C:\CCStudio_v3.3\C6000\cgtools\lib\rts67plus.lib', member'boot.obj' is of unknown type。这个错误怎么办呀。呵呵

  • 这是CCS4的工程。

  • 您好Tony:

     omap-l138 ARM端程序应该加载哪个RTS库,是rts32arm9.lib?我加载之后出现了下面的错误:

    undefined                        first referenced

    symbol                              in file

    ---------                        ----------------

    pinit                            C:\CCStudio_v3.3\tms470\cgtools\lib\rts32arm9.lib

    cinit                            C:\CCStudio_v3.3\tms470\cgtools\lib\rts32arm9.lib

    >>   error: symbol referencing errors - './Debug/omap-l138_int.out' not built

  • 1. 请问是用的CCS4还是CCS3.3?

    2. 请问是哪个工程?

  • hi,Tony

             Boot_DSP_on_SOC_V0.1.zip 很好,很强大,OMAPL138DemoInterrupt 是用CC5开发的,我用ccs4无法使用,可以通过某些设置后直接在CCS4 上使用吗?后来我新建了一个CCS4默认的hello的工程,并加入OMAPL138DemoInterrupt中的src,在仿真的时候跑到_call_swi(327680);就死在那里了,而且无法在handler.asm 中设置断点,设置后显示是灰色,并且有个"!".我想问一下是有什么设置没有设置好吗?如果是,怎么样进行设置,谢谢!

  • viky zhong,请问你的上述问题解决了吗?我在官方的开发板上跑ARM程序是可以的,也能够进中断,但是在自己做的板子上遇见跟你一样的问题,不知道能否帮忙解答一下,谢谢

  • hi,xiaobin,在工程属性的ccs build中,把output fomat 改成legacy COFF 即可解决问题

  • 你好:我用的是ccs4.2,我按照上面的工程,在CCS4.2中测试了arm加载dsp,但是dsp没有启动

    (1)当我不屏蔽掉switch_to_privileged_mode();,的时候程序打印出 cannot open the file,当我屏蔽掉switch_to_privileged_mode();程序可以执行完毕,但是dsp没有启动。我认为switch_to_privileged_mode();不应该被屏蔽掉,但是为什么,有了这个语句之后会打不开dsp的文件呢

    (2)另外,那位有ccs4.2的类似程序,能给我参考一下,邮箱 ytuxiaobin@163.com

  • 关于上面的问题,我找到原因了,switch_to_privileged_mode();会对file的指针造成影响,另外现在arm能够加载dsp,而且dsp也能够运行,但是要求的前提是uboot没有加载,这个比较麻烦,大家有遇见这个情况吗?

  • winteliang您好,我也出现了这样的问题,但是我不知道添加 楼下说的reset DSP,麻烦你和我说说,谢谢

  • tony,您好,我运行Boot_DSP_on_SOC_V0.1.zip里的程序,烧写 .bin(ubl_spi.out和一个点亮LED的程序用AIS工具生成的的),我断电后LED并没有点亮,单独运行时LED能点亮,请问我的问题出在哪了? 楼上有位仁兄说reset DSP,可我没有找到唤醒DSP的程序,麻烦指点下我,唤醒DSP的程序在哪,谢谢。。。

  • 这个demo是讲如何通过ROM bootloader一次性加载ARM和DSP的代码,要将ARM与DSP的.out文件通过Aisgen.exe合成一个文件进行烧写,而不是分开烧写,分开烧写的话你可以参考另一个demo,ARM如何加载DSP代码。

    请看一下附带的说明文档。

  • Tony Tang:

    ”一次性加载ARM和DSP的代码,要将ARM与DSP的.out文件通过Aisgen.exe合成一个文件进行烧写“

    (1)这应该理解为烧写只烧写UBL,而UBOOT不是必须的?

    (2)dsp的程序大小是否收到限制?

  • 1. 用Linux自然要UBOOT,从芯片的角度,只负责将用户代码加载运行起来,后面的过程则由用户实现了。

    2. 没有。

  • tony tang:

    你好,我看了你的那个“分开加载dsp和arm”这个程序我能够在仿真环境下修改以适合我购买的合纵达开发板,实验的结果是能够在仿真环境下实现ARM对DSP的唤醒,dsp也能够正确运行。

    另外我也看了你的“一次性加载ARM和DSP的代码”,这个代码中dsp的程序是用bios下的,我对bios不熟悉,所以修改了你给出的OMAPL138_INT_DSP这个程序,代码的执行设定了在了与ARM不重合的shared RAM中,然后用AISGEN将arm的OUT文件与其相连合成一个,但是烧写的结果是ARM的程序可以运行,而dsp的程序没有运行,试着修改了多次,仍然没有成功,所以有几个问题想请教一下:

    (1)ARM与dsp一起烧写是否要求dsp的程序要是dsp bios的?

    (2)我使用的nand write烧写程序,是由合纵达提供,烧写的nand flash,他是将程序烧写到了nand flash第一个block,这里的位置是否有问题?

    (3)我看了你的dsp bios的那个程序(文件夹 dsp),里面的程序的入口地址是0x11800000,ARM程序的入口地址是0x8000412c,这两个程序的在两个不同的ram中,这里我不大理解,arm的RBL能够把烧写的程序加载到两个不同的RAM中吗?关于这方面的文档资料有哪些?能否给个链接?

    (4)烧写的时候对nand write的烧写方式有什么特殊要求吗?

    (5)关于我以上的调试过程,你能否给几个调试的建议

    谢谢

  • Tony Tang:

    另外你能否把你使用的FLASH 烧写程序给我发一份

    我的邮箱是ytuxiaobin@163.com

    谢谢

  • Hi Tony

    附件里的Boot_DSP_on_SOC_V0.1.zip 无法下载了,麻烦您给我发一份。谢谢。gha20028@163.com

  • Hi Tony

    附件里的Boot_DSP_on_SOC_V0.1.zip 无法下载了,麻烦您给我发一份。谢谢。wangkeyen@163.com

  • tony你好,附件下载不了,麻烦发一份给我,limaosh@tom.com,谢谢。

  • tony你好,附件下载不了,麻烦发一份给我,limaosh@tom.com,谢谢

  •  

    Tony Tang 你好,

    附件里的Boot_DSP_on_SOC_V0.1.zip 无法下载了,麻烦您给我发一份。谢谢。zhouweisun@qq.com

  •          xiaobin你好,“一次性加载ARM和DSP的代码”这个程序你解决了吗?我也遇到这个问题

  •      Tony Tang你好,你贴出来的nand-writer-03.20.00.08.tar.gz 可以在我的板子上运行,你写的例子OMAPL138_DSPL2BOOT是用的SPIFLASH,若要改为NANDFLASH上boot,AISgen for D800K008上的配置需要怎么修改呢(尤其是CS3 setup,设为0x00000012不知对不对)?

    我用的SEED_DEC138开发板,nandflash型号K9F4G08U0A。

  • Tony Tang:

                           我现在在单核芯片C6746上实现二次加载DSP应用程序,根据你的文档“How to boot ARM+DSP SOC”,我先将DSP的.out文件通过hex6x.exe转换成.bin,boot引脚设置为SPI Flash启动,一上电后,存放在SPI Flash的secondry-bootloader程序正确行动,并将存放在FLASH芯片上的bin文件搬运到指定的位置,这些功能都完成实现,并正确执行。                        

    现在问题是:将DSP应用程序的指定到片内存放时(通过修改CMD文件,应用程序存放地址且不与secondary-bootloader程序存放地址重叠),程序能成功跳转到DSP应用程序,并成功运行。一旦将DSP应用程序存放在DDR位置时,程序无法跳转到DSP应用程序的EntryPoint位置,不知道是何原因,麻烦指点一下。另外看了“How to boot ARM+DSP SOC”文档的page10 "Use DM6437 BSL LED demo, get entry point from map file; and memory content from CCS memory view for later AIS file content comparison."我不明白你这句话的目的是什么,.bin文件最前面四个字节已经指明了entry point ,为何还要从.map文件获取?不太理解。

  • Jie,

    #1. 流程能跑通过,说明操作步骤是正确的。

    #2. link到DDR上运行不起来,说明DDR配置不正确。

       A.   确保在AISgen.exe的GUI界面里配置正确的DDR参数,PLL等。

       B.   在second bootloader里不要再配置DDR,PLL等。

    #3. boottable的头4个字节是entry point,AIS的文件头不包括这个信息,是在文件尾。目的只是为了说明一下,能找到就好。

  • wei zhou1 说:

    你贴出来的nand-writer-03.20.00.08.tar.gz 可以在我的板子上运行,你写的例子OMAPL138_DSPL2BOOT是用的SPIFLASH,若要改为NANDFLASH上boot,AISgen for D800K008上的配置需要怎么修改呢(尤其是CS3 setup,设为0x00000012不知对不对)?

    我用的SEED_DEC138开发板,nandflash型号K9F4G08U0A。

    默认配置即可运行,如果想优先时序,提高速度,可以参考NAND的时序配置工具:http://processors.wiki.ti.com/index.php/Programming_Asynchronous_EMIF_on_OMAP-L13x_/_C674x_/_AM1x

     

  • Tony:

    Step1:
    我将Secondary_bootloader.out通过AISgen.exe生成AIS_boot.bin,在AIS的GUI界面中,确实没有配置PLL及DDR参数,但是在bootloader程序有对PLL及DDR进行初始化操作.

    Step2:
    将AIS_boot.bin烧写到SPI Flash首地址中,配置boot引脚为SPI FLASH启动,重新上电后,Secondary_bootloader能成功运行,并输出调试信息,以及DDR的读写测试信息均正常,说明在Secondary_bootloader已经正确配置了PLL及DDR.

    Step3:
    将DSP应用程序.out通过hex6x.exe工具转换成.bin文件,烧写到Flash另一位置。

    Step4:
    重新上电,Secondary_bootloader程序运行,并输出调试信息,并将DSP应用程序.bin文件搬运到指定位置,搬运完成后,执行跳转指定到Entry_point处。

    测试结果:
    DSP应用程序的cmd将代码全部指定分配在片内时,可以得到预期结果,将cmd部分代码分配到DDR时,跳转不成功。

    这是整个测试流程,不知道哪里存在问题,请帮忙看一看,搞了一周多了,都没有什么眉目。

  • 那可以通过:

    #1. 用仿真器调试可以走通整个过程吗?

    #2. 在第二步里,能确定加载成功了吗?

    这个总结的主要目的就是帮助定位启动不成功的原因,你不是前面还问了为什么要看 入口地址吗?

  • Tony:
    在上面的步骤中,第二步是可以完成确认的,通过串口输出的调试信息符合预期,另外通过仿真器来运行的话,也是一样的结果,即DSP应用程序的cmd将代码全部指定分配在片内时,可以得到预期结果,将cmd部分代码分配到DDR时,跳转不成功。

    基于你昨天给我的一些建议,我不仅在bootloader程序中,有对PLL及DDR的初始化,在AISgen的GUI界面中,同时也对PLL1及DDR进行了初始化。这样的话,跳转到仅7K大小LED闪亮程序(代码分配在DDR),这时运行成功了。但是我用一个64K的另一程序替代LED闪亮程序时,程序依旧无法运行。

    现在我有二个疑问:1、在我前面的一些测试中,尽管没有在AISgen的GUI对PLL及DDR进行初始化操作,但是bootloader程序能对DDR正确读写测试的情况下,为何无法运行代码分配在DDR的应用程序。
    2、为何现在小程序可以在DDR可以运行,大程序无法在DDR运行(大程序通过仿真器运行是没有问题的)。是不是我将bootloader程序都分配在片内存储区上(共40个K),所以小程序没问题,大程序就有问题了么?

  • Tony:

             现在都搞好了,谢谢你的建议!

  • Tony Tang 你好。我找了几天关于6416的TCP协处理器SA模式的CSL例程 ,都没有找到。你能帮助我,找到这个CSL的例程吗?

  • Gang,

    建议到这上版块上问一下,C6416是他们在维护支持:

    http://www.deyisupport.com/question_answer/dsp_arm/c6000_multicore/f/53.aspx

  • Tony,你好1

    我下载了你提供的代码包,其中OMAPL138DemoInterrupt导入CCS可以正常编译调试,但是导入OMAPL138_INT_DSP工程的时候,出现了问题:

    提示错误消息:

    See details below.
    Error: Import failed for project 'OMAPL138_INT_DSP' because its meta-data cannot be interpreted. Please contact support.

    我的CCS版本是

    Version: 5.2.1.00018

    是版本兼容的问题吗?

  • 应该是版本的问题,可以将源码再重新建立一个工程,如果还有问题,请提出来。

  • Tony 你好,我在SEED公司的DEC-138开发板上加载了你发布的OMAPL138DemoInterrupt工程,但是编译时出现找不到CPU PRU0和PRU1的驱动,请问什么原因,另外是不是该工程只需在CCS下就可以实现两核的互相控制?我的CCS版本是5.2.1.00018

  • 这个是仿真器的配置,与工程本身无关。

  • 请指点一下在合众达138开发板上应该如何修改
  • 你好!Tony Tang

    现在我在OMAPL138上只用DSP核,不用ARM9;用了你的例程Boot_DSP_on_SOC_V0.1;可以正常启动了。有几个疑问想请教你:

    对这两个文件有点疑惑:1.Boot_DSP_on_SOC_V0.1\OMAPL138_DSPL2BOOT\dsp\Mp3Postproc_omapl138cfg.cmd;2.

    Boot_DSP_on_SOC_V0.1\OMAPL138_DSPL2BOOT\dsp\myboot.asm

    1.myboot.asm文件是进入C语言环境的参数设置,cmd文件中入口地址一定要设置为0x11800000么?

    2.Mp3Postproc_omapl138cfg.cmd 的 .text  ..cinit 可以分配到DDR2的空间地址么,我设置到这个地址,是用不了;地址一定要设置为0x11800080开始么?

  • Hi,jie li

    我也遇到你这个问题,请问怎么解决的呢?求指教,我QQ:2738482551

    谢谢!

  • #1. DSP程序的入口地址设置为1Kbyte地址对齐即可,任何地址空间都可以。

    #2. 程序可以分配到任何地址空间,如果是分配到DDR2,则需要在AISgen的界面里将DDR的配置参数正确填上。

  • HI,Tony Tang

         我目前使用一次性加载ARM和DSP代码烧写进Nor Flash没有问题,并且在DSP代码中实现了通过USB进行代码在线升级,现在有个问题是如果在升级的过程中突然断电的话,因为升级时会擦除flash操作,那样芯片就不能工作了,因为板子做好后是封闭在一个盒子里,只有一个USB接口出来的,不知道有没有什么更好的在线升级方式呢?谢谢!

  • HuiPeng,

    根据你描述的需要,我建议你用ARM加载启动DSP的方式,并且做一个小的系统boot代码来负责加载应用,和升级。升级时只升级应用程序,系统boot不变,这样保证升级失败后,还是可以重新再来一遍的。

    另外这个芯片支持UART烧写,不知道对你是否适用?

  • HI,

    UART的话只能拆开盒子来升级,那样就不方便了,再研究下用ARM加载启动DSP的方式看看,另外做一个小的系统boot,这个有没有相关例程呢?