This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368-IPNC的音频问题



最近使用dm368-ipnc的音频功能时发现,输入如下:

root@192:~# aplay -Dplug:dmix /opt/ipnc/alarm_2_8k.wav
ALSA lib pcm_dmix.c:1018:(snd_pcm_dmix_open) unable to open slave
aplay: main:660: audio open error: Device or resource busy

我尝试过在create文件~/.asoundrc,并添加了如下内容:

pcm.!default { 
type hw 
card EVM 
ctl.!default { 
type hw 
card EVM }
但还是没用,

root@192:~# aplay -l
**** List of PLAYBACK Hardware Devices ****
card 0: EVM [DaVinci DM365 EVM], device 0: CQ93 cq93vc-hifi-0 []
Subdevices: 0/1
Subdevice #0: subdevice #0

在menuconfig里的DM365 codec select里有两个选项,一个是cq93vc,另一个是aic3101,内核默认的是cq,而当我选aic3101后,ipnc启动日志里就会出现

ALSA lib pcm_hw.c:1401:(_snd_pcm_hw_open) Invalid value for card

谁能帮小弟解决ipnc的音频问题啊