在CCS3,.3环境下,用仿真器连上ARM核后,调试GEL文件(开发板自带,仿真器厂家提供的版本问题相同)发现问题如下:配置PLL0失败,每次都是最后一步的时候不能将PLL0改回正常模式(非BYPASS),测量信号,自己的板子与开发板基本上完全相同。如果用FLASH启动方式,烧写..ais.bin和u_boot.bin,后启动显示CHIP INITIATION FAILED ,不知道什么原因,请专家指教。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
补充:连接ARM核正常,
Clear_Memory_Map();
Setup_Memory_Map();
操作也正常
Set_Core_300MHz()时调用下面函数出现问题:
device_PLL0(unsigned int CLKMODE, unsigned int PLLM, unsigned int POSTDIV,unsigned int PLLDIV1, unsigned int PLLDIV2, unsigned int PLLDIV3, unsigned int PLLDIV7 ) {
unsigned int i=0;
/* Clear PLL lock bit */
CFGCHIP0 &= ~(0x00000010);
/* Set PLLENSRC '0',bit 5, PLL Enable(PLLEN) selection is controlled through MMR */
PLL0_PLLCTL &= ~(0x00000020);
......
.....
/*Set the PLLEN bit in PLLCTL to 1 to remove the PLL from bypass mode*/
PLL0_PLLCTL |= 0x1;//这里会出现问题 只要前面做了相关配置,最后两句执行时CCS就会报错
/* SET PLL lock bit*/
CFGCHIP0 |= (0x1 << 4) & 0x00000010;//这里会出现问题
}
补充:连接ARM核正常,
Clear_Memory_Map();
Setup_Memory_Map();
操作也正常
Set_Core_300MHz()时调用下面函数出现问题:
device_PLL0(unsigned int CLKMODE, unsigned int PLLM, unsigned int POSTDIV,unsigned int PLLDIV1, unsigned int PLLDIV2, unsigned int PLLDIV3, unsigned int PLLDIV7 ) {
unsigned int i=0;
/* Clear PLL lock bit */
CFGCHIP0 &= ~(0x00000010);
/* Set PLLENSRC '0',bit 5, PLL Enable(PLLEN) selection is controlled through MMR */
PLL0_PLLCTL &= ~(0x00000020);
......
.....
/*Set the PLLEN bit in PLLCTL to 1 to remove the PLL from bypass mode*/
PLL0_PLLCTL |= 0x1;//这里会出现问题 只要前面做了相关配置,最后两句执行时CCS就会报错
/* SET PLL lock bit*/
CFGCHIP0 |= (0x1 << 4) & 0x00000010;//这里会出现问题
}

执行的GEL代码和输出结果如下(同时有上面的错误提示):
device_PLL0(unsigned int CLKMODE, unsigned int PLLM, unsigned int POSTDIV,unsigned int PLLDIV1, unsigned int PLLDIV2, unsigned int PLLDIV3, unsigned int PLLDIV7 ) {
unsigned int i=0;
GEL_TextOut("\tdevice_PLL0 in............\n","Output",1,1,1);
/* Clear PLL lock bit */
CFGCHIP0 &= ~(0x00000010);
GEL_TextOut("\tCFGCHIP0 &= ~(0x00000010);\n","Output",1,1,1);
/* Set PLLENSRC '0',bit 5, PLL Enable(PLLEN) selection is controlled through MMR */
PLL0_PLLCTL &= ~(0x00000020);
/* PLLCTL.EXTCLKSRC bit 9 should be left at 0 for Freon */
PLL0_PLLCTL &= ~(0x00000200);
/* Set PLLEN=0 to put in bypass mode*/
PLL0_PLLCTL &= ~(0x00000001);
/*wait for 4 cycles to allow PLLEN mux switches properly to bypass clock*/
for(i=0; i<PLLEN_MUX_SWITCH; i++) {;}
/* Select the Clock Mode bit 8 as External Clock or On Chip Oscilator*/
PLL0_PLLCTL &= 0xFFFFFEFF;
PLL0_PLLCTL |= (CLKMODE << 8);
GEL_TextOut("\tPLL0_PLLCTL |= (CLKMODE << 8);\n","Output",1,1,1);
/*Clear PLLRST bit to reset the PLL */
PLL0_PLLCTL &= ~(0x00000008);
/* Disable the PLL output*/
PLL0_PLLCTL |= (0x00000010);
/* PLL initialization sequence
Power up the PLL by setting PWRDN bit set to 0 */
PLL0_PLLCTL &= ~(0x00000002);
/* Enable the PLL output*/
PLL0_PLLCTL &= ~(0x00000010);
/*PLL stabilisation time- take out this step , not required here when PLL in bypassmode*/
for(i=0; i<PLL_STABILIZATION_TIME; i++) {;}
/*Program the required multiplier value in PLLM*/
PLL0_PLLM = PLLM; /* Make PLLMULTIPLEIR as bootpacket*/
GEL_TextOut("\t PLL0_PLLM = PLLM;\n","Output",1,1,1);
/* Prediv setup -Not required */
// PLL0_PREDIV = 0x8000 | PREDIV; /* Make POSTDIV as bootpacket*/
/*If desired to scale all the SYSCLK frequencies of a given PLLC, program the POSTDIV ratio*/
PLL0_POSTDIV = 0x8000 | POSTDIV; /* Make POSTDIV as bootpacket*/
/*Check for the GOSTAT bit in PLLSTAT to clear to 0 to indicate that no GO operation is currently in progress*/
while(PLL0_PLLSTAT & 0x1==1){}
/*Program the RATIO field in PLLDIVx with the desired divide factors. In addition, make sure in this step you leave the PLLDIVx.DxEN bits set so clocks are still enabled (default).*/
PLL0_PLLDIV1 = 0x8000 | PLLDIV1; /* Make PLLDIV1 as bootpacket, do it for other PLLDIVx to if required*/
PLL0_PLLDIV2 = 0x8000 | PLLDIV2;
PLL0_PLLDIV4 = 0x8000 | (((PLLDIV1+1)*4)-1);
PLL0_PLLDIV6 = 0x8000 | PLLDIV1;
PLL0_PLLDIV3 = 0x8000 | PLLDIV3; /* Make PLLDIV3 as bootpacket, do it for other PLLDIVx to if required*/
PLL0_PLLDIV7 = 0x8000 | PLLDIV7; /* Make PLLDIV7 as bootpacket, do it for other PLLDIVx to if required*/
GEL_TextOut("\t PLL0_PLLDIV7 = 0x8000 | PLLDIV7;\n","Output",1,1,1);
/*Set the GOSET bit in PLLCMD to 1 to initiate a new divider transition.*/
PLL0_PLLCMD |= 0x1;
/*Wait for the GOSTAT bit in PLLSTAT to clear to 0 (completion of phase alignment).*/
while(PLL0_PLLSTAT & 0x1==1) { }
/*Wait for PLL to reset properly. See PLL spec for PLL reset time - This step is not required here -step11*/
for(i=0; i<PLL_RESET_TIME_CNT; i++) {;} /*128 MXI Cycles*/
GEL_TextOut("\t for(i=0; i<PLL_RESET_TIME_CNT; i++)\n","Output",1,1,1);
/*Set the PLLRST bit in PLLCTL to 1 to bring the PLL out of reset*/
PLL0_PLLCTL |= 0x8;
GEL_TextOut("\t PLL0_PLLCTL |= 0x8;\n","Output",1,1,1);
/*Wait for PLL to lock. See PLL spec for PLL lock time*/
for(i=0; i<PLL_LOCK_TIME_CNT; i++) {;} /*Make PLL_LOCK_TIME_CNT as boot Packet*/
/*Set the PLLEN bit in PLLCTL to 1 to remove the PLL from bypass mode*/
PLL0_PLLCTL |= 0x1;
GEL_TextOut("\t PLL0_PLLCTL |= 0x1;\n","Output",1,1,1);
/* SET PLL lock bit*/
CFGCHIP0 |= (0x1 << 4) & 0x00000010;
GEL_TextOut("\t CFGCHIP0 |= (0x1 << 4) & 0x00000010;dayinut",1,1,1);
}
打印结果如下:
device_PLL0 in............
CFGCHIP0 &= ~(0x00000010);
PLL0_PLLCTL |= (CLKMODE << 8);
PLL0_PLLM = PLLM;
PLL0_PLLDIV7 = 0x8000 | PLLDIV7;
for(i=0; i<PLL_RESET_TIME_CNT; i++)
PLL0_PLLCTL |= 0x8;
PLL0_PLLCTL |= 0x1;