This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助TI员工



您好!

       我是NDK使用的新手(我使用的开发板是OMAPL137的,使用了c6747这个核),按照NDK的要求配置完成,但是在测试NDK的例子helloworld时,出现如下情况:

TCP/IP Stack 'Hello World!' Application

Using MAC Address: 00-01-02-03-04-05
EMAC should be up and running 
EMAC has been started successfully
Registeration of the EMAC Successful
Service Status: DHCPC : Enabled : : 000
Service Status: DHCPC : Enabled : Running : 000
Link Status: 100Mb/s Full Duplex on PHY 1
Service Status: DHCPC : Enabled : Fault : 002

我查找了很多解决方法,但是几个月过去还是没进展,希望得到您的帮助,谢谢您!