因为项目的需要,我需要用到6657,但是之前并没有接触过DSP,感到很陌生,虽然看了一些TI的资料,关于SYS/BIOS的,MCSDK的,RTSC的,但是还是感觉无从下手写程序。我的程序已经在PC上写好了,就等一直到DSP上,请问下一步应该怎么办呢,从哪里入手呢?谢谢了!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如果你需要做驱动开发,建议你下载K1_STK包和MCSDK,K1_STK可以在http://www.deyisupport.com/question_answer/dsp_arm/c6000_multicore/f/53/t/47664.aspx
下载,看一看这些源代码是怎么写的。
如果你需要做算法部分的开发,那么你需要学习C6000优化的内容,现在TI的编译器对C的优化已经非常完善。
我前面接触过一些多核的开发,如果你愿意的话,可以联系mobilefone@163.com
我正好想了解一些6657的工程应用,看看能否互相提供点有用的信息
你好。
我的邮箱是sunsining1990@163.com. 可以多交流一下开发的经验。谢谢!
Allen Yin,您好!
之前做6678,驱动参考keystone例程,现在需要用6657,想请问两者之间区别大吗?驱动可以稍微修改后直接用吗?还是需要完全重新开发?非常感谢!
驱动大部分都是一样的,当然寄存器基址会有所不同。
比较大的不同的EMAC接口,6657和6678不一样,你可以参考首页的6657 的 STK 进行开发。