Other Parts Discussed in Thread: TPS51200, OMAP-L138
请教专家,我的电路中拟使用6674,但是不使用片上的DDR3外设。667X的硬件设计指南中说,即便DDR3外设不使用时,它的PLL电源AVDDA2仍然要接1.8V电源和加磁珠隔离,时钟输入按照推荐上下拉,VREFSSTL仍然要连接到0.75V VREF;没有提到DDR3的1.5V I/O电源还要不要接,这个应该怎么处理?
另外,看到研华的TMDXEVM5578L电路中,参考电压0.75V的VREF是用1.5V用两个1%的电阻分压得到的;其中使用电源芯片TPS51200产生的0.75V的电源,反而没有接到VREF;是不是我也可以用其他电源通过电阻分压得到0.75V给DDR3做参考电压。TPS51200还是sink/source的LDO,6678不会也跟OMAP-L138一样存在上电时判断接口电平,有漏电流的问题吧?
谢谢。