This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678启动时HyperLink的配置

两片C6678使用HyperLink通讯,因为两片DSP上电程序加载不同步,出现HyperLink配置失败,通讯无法建立的问题。请教下:

两片DSP启动不同步条件下,两端HyperLink配置应该是怎样的时序?

  • 同步加载时没有问题吗?如果同步加载也有问题可能要检查硬件信号.

    如果只是不同步才有问题的话,可以尝试以下:

    1, 在通过PSC使能HyperLink Power domain/module后加5ms时延

    2, 配置HyperLink Serdes时,把寄存器CFGPLL最后配