This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

img64x.lib库的问题



我用的DM648,采用bios,有图像采集程序任务和图像处理,图像处理任务采用TI函数库img64x.lib中的IMG_sobel(unsigned char *in,unsigned char *out,int col,int row),其中将in和out通过#pragma DATA_SECTION在DDR中开辟两个数组空间,其中图像处理任务中连续调用两次IMG_sobel函数,col和row分别为160,160,最好运行系统程序时,图像采集程序老是跑飞,而换成TI的C代码后,即调用IMG_sobel_c(unsigned char *in,unsigned char *out,int col,int row)时,则程序没有问题,是不是IMG_sobel()库函数有什么设置要求啊,还有当用IMG_sobel()库函数时,col和row为80和80时系统运行也没问题,求解,谢谢