demo板上6657用CDCE62005RGZT做时钟配置。但dsp的HyperLink ,SRIO,SGMII功能不需要,相应的时钟要不要给?如果不要给,能否推荐一个时钟芯片?另外62005要通过spi做时钟配置,能不能推荐一个将输出时钟锁定的,不需要通过编程接口配置的时钟芯片?因为不想通过spi配置。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
demo板上6657用CDCE62005RGZT做时钟配置。但dsp的HyperLink ,SRIO,SGMII功能不需要,相应的时钟要不要给?如果不要给,能否推荐一个时钟芯片?另外62005要通过spi做时钟配置,能不能推荐一个将输出时钟锁定的,不需要通过编程接口配置的时钟芯片?因为不想通过spi配置。谢谢!
您好,
对于不需要的CLK PIN设计参考硬件设计手册
http://www.ti.com/product/tms320c6657
application notes -> hardware design guide for keystone devices
->clocking design guide for keystone devices
建议将时钟芯片选择的问题发送到 接口/时钟子论坛:http://www.deyisupport.com/question_answer/analog/interface_and_clocks/f/59.aspx