This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TCP3dD不能正确返回译码结果的问题



是关于一个TCP3D程序在C6670评估板能运行,但是在vadatech的VT864机箱上AMC—2C6670不能运行的问题,具体参见word文档的描述,测试程序也一起添加到了附件。

tcp测试程序和问题.zip
  • 两个板子的测试方法有什么区别么,都是通过CCS链接仿真器将程序load 到DSP上运行么?

    使用EVM时有运行gel文件进行初始化PLL么,在机箱上有根据输入core clock修改PLL的配置么?可以查看Core PLL的寄存器确认是否配置了主锁相环时钟。

  • 两种测试方法的主要差别有两个:一个是仿真器不一样,C6670评估版用的是560v2的仿真器,vt864机箱用的是100v2的仿真器;另外一个差别就是导入的gel文件不一样。其他的操作都是一样,都是在ccs5.3版本上load到DSP运行,而且bcp和fftc的协处理器都是可以正常运行的,就是tcp的出了问题。

  • 首先确认一下TCP3D PSC是否使能,然后依次确认输入输出EDMA是否将数据搬移到TCP3D内部memory。