This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 GEL文件加载失败问题



自制C6678板,CORE、DDR、PA三个时钟与EVM相同,已通过示波器看到,在加载EVM的GEL发生错误。不加载GEL文件时,在1GHz能运行程序,测试的串口程序数据收发都正常,但单步DEBUG时经常在设置完main PLL时出现memory不能read的情况,跟加载GEL时出现的问题很相似。以下是GEL输出:

C66xx_0: GEL Output: Setup_Memory_Map...
C66xx_0: GEL Output: Setup_Memory_Map... Done.
C66xx_0: GEL Output:
Connecting Target...
C66xx_0: GEL Output: DSP core #0
C66xx_0: GEL Output: C6678L GEL file Ver is 1.6
C66xx_0: GEL Output: Setup Cache...
C66xx_0: GEL Output: L1P = 32K
C66xx_0: GEL Output: L1D = 32K
C66xx_0: GEL Output: L2 = ALL SRAM
C66xx_0: GEL Output: Setup Cache... Done.
C66xx_0: GEL Output: PLL1 Setup...
C66xx_0: GEL Output: PLL1 Setup for DSP @ 1000.0 MHz.
C66xx_0: GEL Output: SYSCLK2 = 333.3333 MHz, SYSCLK5 = 200.0 MHz.
C66xx_0: GEL Output: SYSCLK8 = 15.625 MHz.
C66xx_0: GEL Output: PLL1 Setup... Done.
C66xx_0: GEL Output: Power on all PSC modules and DSP domains...
C66xx_0: Trouble Reading Memory Block at 0x2350810 on Page 0 of Length 0x4: (Error -1202 @ 0x2350810) Device core is hung. The debugger will attempt to force the device to a ready state to recover debug control. Your application's state will be corrupt. You should have limited access to memory and registers, but you may need to reset the device to debug further. (Emulation package 5.0.569.0)
C66xx_0: GEL: Error while executing OnTargetConnect(): target access failed at (*(mdstat)&0x1f) [evmc6678l.gel:1322] at Set_PSC_State(0, 4, 0x3) [evmc6678l.gel:1744] at Set_Psc_All_On() [evmc6678l.gel:900] at Global_Default_Setup_Silent() [evmc6678l.gel:628] at OnTargetConnect() .
C66xx_0: GEL Output: Invalidate All Cache...

C66xx_0: Trouble Writing Memory Block at 0x1845028 on Page 0 of Length 0x4: (Error -1202 @ 0x1845028) Device core is hung. The debugger will attempt to force the device to a ready state to recover debug control. Your application's state will be corrupt. You should have limited access to memory and registers, but you may need to reset the device to debug further. (Emulation package 5.0.569.0)
C66xx_0: Trouble Reading Memory Block at 0x1845048 on Page 0 of Length 0x4: (Error -1060 @ 0x1845048) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.0.569.0)
C66xx_0: GEL: Error calling OnPreFileLoaded(): target access failed at (*((int *) (0x01840000+0x5048))&0x0001) [evmc6678l.gel:1883] at Invalidate_Cache() [evmc6678l.gel:678] at OnPreFileLoaded()
C66xx_0: Trouble Reading Memory Block at 0x800000 on Page 0 of Length 0x4: (Error -1060 @ 0x64) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.0.569.0)
C66xx_0: File Loader: Data verification failed at address 0x00800000 Please verify target memory and memory map.