This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6747,mcasp + edma3无法正常首发数据



我用mcasp的tdm模式配置i2s,然后用edma3来传输数据,但是目前还不能正确传输。

edma3配置如下:

void EDMA3_SendInitialCfg(void)
{
edma3ccRegs->EMCR = (Uint32) 0x0002;
edma3ccRegs->SECR = (Uint32) 0x0002;

edma3ccRegs->EESR = (Uint32) 0x0002;
//edma3ccRegs->DRA[1].DRAE=(Uint32) 0x0002;
edma3ccRegs->DMAQNUM[0] = (CSL_EDMA3CC_DMAQNUM_E1_Q0 << CSL_EDMA3CC_DMAQNUM_E1_SHIFT);

edma3ccRegs->PARAMSET[1].OPT = (CSL_EDMA3CC_OPT_TCINTEN_ENABLE << CSL_EDMA3CC_OPT_TCINTEN_SHIFT)|\
(0x01 << CSL_EDMA3CC_OPT_TCC_SHIFT)|\
(CSL_EDMA3CC_OPT_SYNCDIM_ASYNC << CSL_EDMA3CC_OPT_SYNCDIM_SHIFT);
edma3ccRegs->PARAMSET[1].SRC = (Uint32) &xmt;

edma3ccRegs->PARAMSET[1].A_B_CNT = (Uint32) 0x00020004;

edma3ccRegs->PARAMSET[1].DST = 0x01D00000;//XBUFADD; //XBUF地址(通道目的地址)

edma3ccRegs->PARAMSET[1].SRC_DST_BIDX = (0x0000 << CSL_EDMA3CC_SRC_DST_BIDX_DSTBIDX_SHIFT)|\
(0x0004 << CSL_EDMA3CC_SRC_DST_BIDX_SRCBIDX_SHIFT);

edma3ccRegs->PARAMSET[1].LINK_BCNTRLD = 0x0002FFFF;

edma3ccRegs->PARAMSET[1].SRC_DST_CIDX = (Uint32)0x04;

edma3ccRegs->PARAMSET[1].CCNT = (Uint32)0x0f;
edma3ccRegs->IESR = (Uint32) 0x0002;

}

void EDMA3_ReceiveStartCfg(void)
{
edma3ccRegs->EMCR = (Uint32) 0x0001;
edma3ccRegs->SECR = (Uint32) 0x0001;

edma3ccRegs->EESR = (Uint32) 0x0001;

edma3ccRegs->DRA[1].DRAE=(Uint32) 0x0001;

edma3ccRegs->DMAQNUM[0] = (CSL_EDMA3CC_DMAQNUM_E0_Q0 << CSL_EDMA3CC_DMAQNUM_E0_SHIFT);

edma3ccRegs->PARAMSET[0].OPT = (CSL_EDMA3CC_OPT_TCINTEN_ENABLE << CSL_EDMA3CC_OPT_TCINTEN_SHIFT)|\
//(CSL_EDMA3CC_OPT_FWID_32BIT << CSL_EDMA3CC_OPT_FWID_SHIFT);
(0x00 << CSL_EDMA3CC_OPT_TCC_SHIFT)|\
(CSL_EDMA3CC_OPT_SYNCDIM_ASYNC << CSL_EDMA3CC_OPT_SYNCDIM_SHIFT);

edma3ccRegs->PARAMSET[0].SRC = 0x01D00000;//RBUFADD; //RBUF地址(通道源地址)

edma3ccRegs->PARAMSET[0].A_B_CNT = (Uint32) 0x00020004;

edma3ccRegs->PARAMSET[0].DST = (Uint32) &rcv;

edma3ccRegs->PARAMSET[0].SRC_DST_BIDX = (0x0004 << CSL_EDMA3CC_SRC_DST_BIDX_DSTBIDX_SHIFT)|\
(0x0000 << CSL_EDMA3CC_SRC_DST_BIDX_SRCBIDX_SHIFT);

edma3ccRegs->PARAMSET[0].LINK_BCNTRLD = 0x0002FFFF;

edma3ccRegs->PARAMSET[0].SRC_DST_CIDX = (Uint32)0x04;

edma3ccRegs->PARAMSET[0].CCNT = (Uint32)0x0f;
edma3ccRegs->IESR = (Uint32) 0x0001;

}

主函数中

while (!(edma3ccRegs->IPR & 0x0002));
mcasp0Regs->XBUF0 = xmt[i];
while (!(edma3ccRegs->IPR & 0x0001));
rcv[i] = mcasp0Regs->RBUF0;

程序死在while (!(edma3ccRegs->IPR & 0x0002));

IPR寄存始终为0,请问哪里配置的有问题,不胜感激!